<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic lpc1343 capture level in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1343-capture-level/m-p/835661#M33340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what is the low/high level for the P1.5 capture&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* For receive, this module uses TMR32B0-CAP0 input (capture and interrupt on both edges) */&lt;BR /&gt;/* TMR32B0-CAP0 input (P1.5) is connected to P1.1 (to check high / low level by software) */&lt;BR /&gt;/* So set P1.5 as CT32B0.CAP0 (= DALI receive pin). Bit 7:6 (reserved) are also set to 1 */&lt;BR /&gt;#define DALI_ConfigInput() { LPC_IOCON-&amp;gt;PIO1_5 = 0xD2; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Jun 2018 01:28:05 GMT</pubDate>
    <dc:creator>googcheng</dc:creator>
    <dc:date>2018-06-30T01:28:05Z</dc:date>
    <item>
      <title>lpc1343 capture level</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1343-capture-level/m-p/835661#M33340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what is the low/high level for the P1.5 capture&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* For receive, this module uses TMR32B0-CAP0 input (capture and interrupt on both edges) */&lt;BR /&gt;/* TMR32B0-CAP0 input (P1.5) is connected to P1.1 (to check high / low level by software) */&lt;BR /&gt;/* So set P1.5 as CT32B0.CAP0 (= DALI receive pin). Bit 7:6 (reserved) are also set to 1 */&lt;BR /&gt;#define DALI_ConfigInput() { LPC_IOCON-&amp;gt;PIO1_5 = 0xD2; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jun 2018 01:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1343-capture-level/m-p/835661#M33340</guid>
      <dc:creator>googcheng</dc:creator>
      <dc:date>2018-06-30T01:28:05Z</dc:date>
    </item>
    <item>
      <title>Re: lpc1343 capture level</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1343-capture-level/m-p/835662#M33341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jay,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the data sheet of the LPC1343 (&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/LPC1311_13_42_43.pdf" title="https://www.nxp.com/docs/en/data-sheet/LPC1311_13_42_43.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/LPC1311_13_42_43.pdf&lt;/A&gt;) if you reference table 7, you will see the information you are looking for.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64831iEDA7C8D6BA22BD0A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jul 2018 19:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1343-capture-level/m-p/835662#M33341</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-07-03T19:48:21Z</dc:date>
    </item>
  </channel>
</rss>