<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4370 - Speed with VCOM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835367#M33330</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using USB0 port of my LPC4370 as a virtual com.&lt;/P&gt;&lt;P&gt;In this case, which is the speed of the USB communication?&lt;/P&gt;&lt;P&gt;Full speed or High speed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mattia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Aug 2018 10:12:14 GMT</pubDate>
    <dc:creator>mattiad</dc:creator>
    <dc:date>2018-08-29T10:12:14Z</dc:date>
    <item>
      <title>LPC4370 - Speed with VCOM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835367#M33330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using USB0 port of my LPC4370 as a virtual com.&lt;/P&gt;&lt;P&gt;In this case, which is the speed of the USB communication?&lt;/P&gt;&lt;P&gt;Full speed or High speed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mattia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 10:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835367#M33330</guid>
      <dc:creator>mattiad</dc:creator>
      <dc:date>2018-08-29T10:12:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 - Speed with VCOM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835368#M33331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB0 supports all high-speed, full-speed, and low-speed USB-compliant peripherals.&lt;/P&gt;&lt;P&gt;If you are using the&amp;nbsp;usbd_rom_cdc_vcom LPCOpen example, then is high speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 14:12:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835368#M33331</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-08-29T14:12:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 - Speed with VCOM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835369#M33332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Soledad!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't understand another thing: in some evaluation boards there are 33Ohm resistances in D+ and D- lines.&lt;/P&gt;&lt;P&gt;In this schematic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/downloads/en/design-support/LPC4330_Xplorer_schematic_OM13027.pdf" title="https://www.nxp.com/downloads/en/design-support/LPC4330_Xplorer_schematic_OM13027.pdf"&gt;https://www.nxp.com/downloads/en/design-support/LPC4330_Xplorer_schematic_OM13027.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;33Ohm are in the USB1 port and not in USB0 port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why in some cases are added and in another cases not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose that fore a Virtual COM link it's better if they are added.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mattia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2018 07:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Speed-with-VCOM/m-p/835369#M33332</guid>
      <dc:creator>mattiad</dc:creator>
      <dc:date>2018-08-30T07:07:24Z</dc:date>
    </item>
  </channel>
</rss>