<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: CAN FD with RxErr</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833880#M33279</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry&lt;/P&gt;&lt;P&gt;That's right.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the error frame occured due to my CAN OE device is VN1630, not compatiable with ISO11898-2015 standard. and when the project change to non-iso mode, no error frame occured;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have the newest CAN instruments to monitor the CANFD frame, maybe no error occured even in ISO mode;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also hope you can feedback a result for the test, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Dec 2018 14:02:50 GMT</pubDate>
    <dc:creator>黎明孟</dc:creator>
    <dc:date>2018-12-29T14:02:50Z</dc:date>
    <item>
      <title>CAN FD with RxErr</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833876#M33275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The offical demo used for CANFD debug, the RxErr occured;&lt;/P&gt;&lt;P&gt;The CAN OE used for the msg monitor and the Rate change to 500K/2M; the 2 nodes connected together; No other CAN node in the network;&lt;/P&gt;&lt;P&gt;You can see that the data also received but with the form error; actually, sometimes report CRC error and sometimes report Stuff bit error;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems something wrong at the Stuff fileld or the CRC field, but i don't know how to fix it!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2018 15:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833876#M33275</guid>
      <dc:creator>黎明孟</dc:creator>
      <dc:date>2018-12-26T15:18:22Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD with RxErr</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833877#M33276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Limeng,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please tell me your LPC chip part number, then I can help you to check the details.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; What the CANFD code you&amp;nbsp; are using, do you try the official code, if you also use the official code, please tell me what the code you are using?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please also tell me what the LPC board you are using, you own designed board or the nxp official board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Waiting for your reply!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2018 03:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833877#M33276</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-12-28T03:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD with RxErr</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833878#M33277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kit ordered from NXP the part is OM13094,uP is 54618 with CAN FD kit;&lt;/P&gt;&lt;P&gt;The project used also from NXP offical example "LPC5461x-CANFD-DriverAPI"--&amp;gt;"fd_msgobjs";&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i change the register "config.enableNonISOMode=true;" The error frame fixed！&lt;/P&gt;&lt;P&gt;So it seems the CANOE version can't support the ISO FD protocol.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also many thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2018 14:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833878#M33277</guid>
      <dc:creator>黎明孟</dc:creator>
      <dc:date>2018-12-28T14:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD with RxErr</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833879#M33278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Liming,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your updated information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you mean, when you use fd_msgobjs project directly without any modification in the CANFD driver, it has error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; But, if you modify the code :&lt;/P&gt;&lt;P&gt;config.enableNonISOMode=true;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; It doesn't have errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Is it right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If yes, i will test it on my side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2018 07:17:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833879#M33278</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-12-29T07:17:27Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD with RxErr</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833880#M33279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry&lt;/P&gt;&lt;P&gt;That's right.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the error frame occured due to my CAN OE device is VN1630, not compatiable with ISO11898-2015 standard. and when the project change to non-iso mode, no error frame occured;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have the newest CAN instruments to monitor the CANFD frame, maybe no error occured even in ISO mode;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also hope you can feedback a result for the test, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2018 14:02:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-with-RxErr/m-p/833880#M33279</guid>
      <dc:creator>黎明孟</dc:creator>
      <dc:date>2018-12-29T14:02:50Z</dc:date>
    </item>
  </channel>
</rss>