<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic a LPC81x ISP problem in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824899#M32982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in trouble with ISP of LPC812.&lt;/P&gt;&lt;P&gt;A command of ISP, "Read &amp;lt;address&amp;gt; &amp;lt;number of byte&amp;gt;" seems to be wired when I read an address, 0x3808, which is the middle of page 224. there is no problem when I read 0x3800, 0x3804 and 0x380C. ISP returns the correct data via UART. But only reading the address of 0x3808, the return data is 0x00000000. Whenever read data, I designate &amp;lt;number of byte&amp;gt; as 4. and keep word boundary.&lt;/P&gt;&lt;P&gt;Is there a bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here below are information of microprocessor I have.&lt;/P&gt;&lt;P&gt;ProductName: LPC812M101JDH20&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 07:48:37 GMT</pubDate>
    <dc:creator>torukoyama</dc:creator>
    <dc:date>2018-07-18T07:48:37Z</dc:date>
    <item>
      <title>a LPC81x ISP problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824899#M32982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in trouble with ISP of LPC812.&lt;/P&gt;&lt;P&gt;A command of ISP, "Read &amp;lt;address&amp;gt; &amp;lt;number of byte&amp;gt;" seems to be wired when I read an address, 0x3808, which is the middle of page 224. there is no problem when I read 0x3800, 0x3804 and 0x380C. ISP returns the correct data via UART. But only reading the address of 0x3808, the return data is 0x00000000. Whenever read data, I designate &amp;lt;number of byte&amp;gt; as 4. and keep word boundary.&lt;/P&gt;&lt;P&gt;Is there a bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here below are information of microprocessor I have.&lt;/P&gt;&lt;P&gt;ProductName: LPC812M101JDH20&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 07:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824899#M32982</guid>
      <dc:creator>torukoyama</dc:creator>
      <dc:date>2018-07-18T07:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: a LPC81x ISP problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824900#M32983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torukoyama,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your interest in NXP LPC product, I would like to provide service for you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I need more information about your question.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Please also provide me your LPC812M101JDH20 marking&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65863iB03DD4CE3AE8A878/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. Please use the flash magic to read out the memory which contains 0X3800-0X38FF.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 3. Please give me the whole ISP command which you are using to connect the LPC812, and read the 0x3800, 0x3804,&amp;nbsp;0x3808 and 0x380C, you can give me the screen shoot from our serial tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your cooperation, then I will do the detail check on my side.&lt;/P&gt;&lt;P&gt;Waiting for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 08:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824900#M32983</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-07-19T08:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: a LPC81x ISP problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824901#M32984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torukoyama,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please check my test result with lpc812max board.&lt;/P&gt;&lt;P&gt;1. Use the flash magic read out the 0x3800 address data:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65877i872219360F43E838/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the data in 0X3800,0X3804,0X3808,0X380C is 0xffffffff.&lt;/P&gt;&lt;P&gt;Please check my ISP mode command:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65878iE60A5D094234A9BB/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;0X52 0X20 0X31 0X34 0X33 0X34 0X34 0X0D 0X0A 0X30 0X0D 0X0A 0XFF 0XFF 0XFF 0XFF&lt;/P&gt;&lt;P&gt;It is:R 0 14344&amp;lt;cr&amp;gt;&amp;lt;lf&amp;gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;0&lt;/STRONG&gt;&lt;/SPAN&gt;&amp;lt;cr&amp;gt;&amp;lt;lf&amp;gt; 0xffffffff&lt;/P&gt;&lt;P&gt;14344: 0x3800&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;0:&lt;SPAN style="color: #000000;"&gt;&lt;STRONG&gt;CMD_SUCCESS&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;&lt;STRONG&gt;0xffffffff: actuall data plain binary&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;You can find, 14344 is address 0x3808, the read out data is 0xffffffff, the same as the result from the flashmagic.&lt;/P&gt;&lt;P&gt;My chip is also LPC812M101JDH20.The revision identifier is 4C.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 10:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/a-LPC81x-ISP-problem/m-p/824901#M32984</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-07-19T10:18:29Z</dc:date>
    </item>
  </channel>
</rss>