<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Brown out BOD voltage levels LPC433x in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Brown-out-BOD-voltage-levels-LPC433x/m-p/823447#M32944</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can somebody help me where to find voltage levels of BOD, both interrupt and reset.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;User manual implicates that there are four levels of BOD voltage threshold, Level 0 to Level 3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;however in data sheet there is are only two levels Level 2 and Level 3 &amp;nbsp;mentioned.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Radomir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jun 2018 12:00:40 GMT</pubDate>
    <dc:creator>radomirkozub-re</dc:creator>
    <dc:date>2018-06-27T12:00:40Z</dc:date>
    <item>
      <title>Brown out BOD voltage levels LPC433x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Brown-out-BOD-voltage-levels-LPC433x/m-p/823447#M32944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can somebody help me where to find voltage levels of BOD, both interrupt and reset.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;User manual implicates that there are four levels of BOD voltage threshold, Level 0 to Level 3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;however in data sheet there is are only two levels Level 2 and Level 3 &amp;nbsp;mentioned.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Radomir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 12:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Brown-out-BOD-voltage-levels-LPC433x/m-p/823447#M32944</guid>
      <dc:creator>radomirkozub-re</dc:creator>
      <dc:date>2018-06-27T12:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Brown out BOD voltage levels LPC433x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Brown-out-BOD-voltage-levels-LPC433x/m-p/823448#M32945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Radomir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I beleive those levels were left out of that datasheet because the reset assertion points are quite far from the minimum operating VDD voltage. But you can still use the values from the LPC4350/30/20/10 datasheet as reference:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/LPC435X_3X_2X_1X.pdf" title="https://www.nxp.com/docs/en/data-sheet/LPC435X_3X_2X_1X.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/LPC435X_3X_2X_1X.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 00:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Brown-out-BOD-voltage-levels-LPC433x/m-p/823448#M32945</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-06-29T00:02:16Z</dc:date>
    </item>
  </channel>
</rss>