<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  LPC214x USB problem with sleep mode in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC214x-USB-problem-with-sleep-mode/m-p/819669#M32815</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="font-size: 11.0pt;"&gt;Lesieur&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;It may me also related to the version of USB controller divers included by Windows. You could take a look to the following links:&lt;/P&gt;&lt;P&gt;&lt;A href="https://answers.microsoft.com/en-us/windows/forum/windows_7-hardware/blue-screen-on-hibernatesuspend-for-windows-7-x64/1367fee5-1b5d-4f3f-8335-56587623b728"&gt;https://answers.microsoft.com/en-us/windows/forum/windows_7-hardware/blue-screen-on-hibernatesuspend-for-windows-7-x64/1367fee5-1b5d-4f3f-8335-56587623b728&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/309556"&gt;https://community.nxp.com/thread/309556&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Aug 2018 22:01:03 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-08-06T22:01:03Z</dc:date>
    <item>
      <title>LPC214x USB problem with sleep mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC214x-USB-problem-with-sleep-mode/m-p/819668#M32814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with the MCU LPC214x (LPC2141) with Windows 7, 64 bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use a usb driver on the MCU and the usb driver &lt;STRONG&gt;&lt;EM&gt;lpc-ucom-vcom.inf&lt;/EM&gt;&lt;/STRONG&gt; provide by NXP for windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the sleep mode. When the microcontroller is connected by USB with the computer and the computer goes to sleep, &lt;BR /&gt;I have this error (BUGCODE_USB_DRIVER, 0X000000FE (0x04,0xFFFFFA8016F19010,0xFFFFFA801888600,0x0FFFFFA801AD92950)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79641iF45C5EF6BD3FB917/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The proporties of the usb driver on the MCU are :&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Power management features:&lt;BR /&gt;00000019&lt;BR /&gt;PDCAP_D0_SUPPORTED&lt;BR /&gt;PDCAP_D3_SUPPORTED&lt;BR /&gt;PDCAP_WAKE_FROM_D0_SUPPORTED&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I think the problem comes from the usb driver on the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to know if the problem comes from the driver on the mcu or on windows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Aug 2018 17:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC214x-USB-problem-with-sleep-mode/m-p/819668#M32814</guid>
      <dc:creator>guillaumelesieu</dc:creator>
      <dc:date>2018-08-05T17:02:35Z</dc:date>
    </item>
    <item>
      <title>Re:  LPC214x USB problem with sleep mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC214x-USB-problem-with-sleep-mode/m-p/819669#M32815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="font-size: 11.0pt;"&gt;Lesieur&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;It may me also related to the version of USB controller divers included by Windows. You could take a look to the following links:&lt;/P&gt;&lt;P&gt;&lt;A href="https://answers.microsoft.com/en-us/windows/forum/windows_7-hardware/blue-screen-on-hibernatesuspend-for-windows-7-x64/1367fee5-1b5d-4f3f-8335-56587623b728"&gt;https://answers.microsoft.com/en-us/windows/forum/windows_7-hardware/blue-screen-on-hibernatesuspend-for-windows-7-x64/1367fee5-1b5d-4f3f-8335-56587623b728&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/309556"&gt;https://community.nxp.com/thread/309556&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2018 22:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC214x-USB-problem-with-sleep-mode/m-p/819669#M32815</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-08-06T22:01:03Z</dc:date>
    </item>
  </channel>
</rss>