<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC2368 + external RAM (61LV256AL)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819665#M32811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I'm looking for an external RAM for LPC2368. My choice - IS61LV256AL. Can I use GPDMA to access external memory? H&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;ow much it fast and difficult?&lt;/SPAN&gt;&lt;/SPAN&gt; Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2018 14:39:51 GMT</pubDate>
    <dc:creator>pazdimpazdim</dc:creator>
    <dc:date>2018-06-26T14:39:51Z</dc:date>
    <item>
      <title>LPC2368 + external RAM (61LV256AL)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819665#M32811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I'm looking for an external RAM for LPC2368. My choice - IS61LV256AL. Can I use GPDMA to access external memory? H&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;ow much it fast and difficult?&lt;/SPAN&gt;&lt;/SPAN&gt; Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 14:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819665#M32811</guid>
      <dc:creator>pazdimpazdim</dc:creator>
      <dc:date>2018-06-26T14:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 + external RAM (61LV256AL)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819666#M32812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the RAM connect to the GPIO?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 14:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819666#M32812</guid>
      <dc:creator>pazdimpazdim</dc:creator>
      <dc:date>2018-06-26T14:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 + external RAM (61LV256AL)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819667#M32813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you are developing a new application, you may consider a newer option, as the LPC2xxx are now part of the legacy devices. Anyway, in case of requiring external RAM, as the LPC2368 doesn’t have external memory controller, there are some cases where external SRAM can be connected with GPIOs, just considering the address, data pins status/impedances. As it may become slow/difficult, another option could be using an external I2C or SPI RAM, using these peripherals already included on the LPC2368.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 20:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-external-RAM-61LV256AL/m-p/819667#M32813</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-06-29T20:05:43Z</dc:date>
    </item>
  </channel>
</rss>