<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC1788 RTC's General purpose registers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-RTC-s-General-purpose-registers/m-p/818442#M32756</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC block includes 20 bytes of &lt;STRONG&gt;battery-powered&lt;/STRONG&gt; backup registers, allowing system status to be stored when the rest of the chip is powered off. Battery power can be supplied from a standard 3 V Lithium button cell.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Aug 2018 13:27:13 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2018-08-23T13:27:13Z</dc:date>
    <item>
      <title>LPC1788 RTC's General purpose registers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-RTC-s-General-purpose-registers/m-p/818441#M32755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I have a question about&amp;nbsp;LPC1788 RTC's General purpose registers 0-4, &amp;nbsp; I write 1 to&amp;nbsp;&lt;SPAN&gt;General purpose registers 0 , then power off(without battery powered) ,&amp;nbsp;General purpose registers 0 value changed to 0 after power on.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;the user manual said : These registers can be used to store import information when the main power supply is off . &amp;nbsp;It seems that&amp;nbsp;General purpose registers can not store information without main power supply &amp;amp; battery power supply?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 03:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-RTC-s-General-purpose-registers/m-p/818441#M32755</guid>
      <dc:creator>lihai</dc:creator>
      <dc:date>2018-08-23T03:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 RTC's General purpose registers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-RTC-s-General-purpose-registers/m-p/818442#M32756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC block includes 20 bytes of &lt;STRONG&gt;battery-powered&lt;/STRONG&gt; backup registers, allowing system status to be stored when the rest of the chip is powered off. Battery power can be supplied from a standard 3 V Lithium button cell.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 13:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-RTC-s-General-purpose-registers/m-p/818442#M32756</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-08-23T13:27:13Z</dc:date>
    </item>
  </channel>
</rss>