<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NVT2008 with pushpull outputs in both sides.  in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NVT2008-with-pushpull-outputs-in-both-sides/m-p/817920#M32747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! &lt;/P&gt;&lt;P&gt;I have an implmementation doubt in regard the usage of this chip.&lt;/P&gt;&lt;P&gt;I have to interfaces a 3.3v domain (microcontroller) witha 5V domain (lcd).&lt;/P&gt;&lt;P&gt;From both sides I have pushpull outputs and hiz inputs.&lt;/P&gt;&lt;P&gt;Do I need pullup resistos on both sides or all the examples from the datasheet are targeting to opendrain outputs?&lt;/P&gt;&lt;P&gt;Table 7, for example, shows minimum pullup resistor values. but in 7.4 "How to size pullup..." exlicits that it is for OD outputs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, somewhere in the datasheet says that for PP outputs pull up resistors mey be required.&lt;/P&gt;&lt;P&gt;With which criteria?&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Sep 2018 11:14:03 GMT</pubDate>
    <dc:creator>francobucafusco</dc:creator>
    <dc:date>2018-09-12T11:14:03Z</dc:date>
    <item>
      <title>NVT2008 with pushpull outputs in both sides.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NVT2008-with-pushpull-outputs-in-both-sides/m-p/817920#M32747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! &lt;/P&gt;&lt;P&gt;I have an implmementation doubt in regard the usage of this chip.&lt;/P&gt;&lt;P&gt;I have to interfaces a 3.3v domain (microcontroller) witha 5V domain (lcd).&lt;/P&gt;&lt;P&gt;From both sides I have pushpull outputs and hiz inputs.&lt;/P&gt;&lt;P&gt;Do I need pullup resistos on both sides or all the examples from the datasheet are targeting to opendrain outputs?&lt;/P&gt;&lt;P&gt;Table 7, for example, shows minimum pullup resistor values. but in 7.4 "How to size pullup..." exlicits that it is for OD outputs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, somewhere in the datasheet says that for PP outputs pull up resistors mey be required.&lt;/P&gt;&lt;P&gt;With which criteria?&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 11:14:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NVT2008-with-pushpull-outputs-in-both-sides/m-p/817920#M32747</guid>
      <dc:creator>francobucafusco</dc:creator>
      <dc:date>2018-09-12T11:14:03Z</dc:date>
    </item>
    <item>
      <title>Re: NVT2008 with pushpull outputs in both sides.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NVT2008-with-pushpull-outputs-in-both-sides/m-p/817921#M32748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Hello, Franco,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;The need for pull-ups resistor depends on the application,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;e.g.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;For Down translation (from Bn to An uni-direction)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Pull-ups resistors may be needed only if the translation VCC(B) - VCC(A) &amp;lt; 1V, on your lower voltage side, be it OD or PP, just to make sure that the voltage high on the low side it is as high as needed, as for your high side no PU are needed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;As for Up translation (from An to Bn uni-direction)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Resistors in both sides may be needed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Please see AN11127 [&lt;A href="https://www.nxp.com/docs/en/application-note/AN11127.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11127.pdf&lt;/A&gt;] for references, page 9, section 5.3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Regards,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Aldo.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 15:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NVT2008-with-pushpull-outputs-in-both-sides/m-p/817921#M32748</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2018-09-13T15:38:29Z</dc:date>
    </item>
  </channel>
</rss>