<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: USB1 ULPI interface on OM13088</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817664#M32738</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Am I correct?&lt;BR /&gt;-- Yes, you're right, you can use USB0 which contains on-chip high-speed UTMI+ compliant transceiver to implement high-speed mode.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jun 2018 02:43:56 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2018-06-27T02:43:56Z</dc:date>
    <item>
      <title>USB1 ULPI interface on OM13088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817663#M32737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I bought OM13088 assuming&amp;nbsp;it had the ULPI interface for USB1 broken out to a header but this doesn't seem to be the case. Am I correct? Is there a way to connect an external PHY to USB1 or am I stuck with FS on that interface?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 23:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817663#M32737</guid>
      <dc:creator>eg0n</dc:creator>
      <dc:date>2018-06-25T23:36:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB1 ULPI interface on OM13088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817664#M32738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Am I correct?&lt;BR /&gt;-- Yes, you're right, you can use USB0 which contains on-chip high-speed UTMI+ compliant transceiver to implement high-speed mode.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 02:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817664#M32738</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-06-27T02:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: USB1 ULPI interface on OM13088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817665#M32739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This project requires 2 HS interfaces. Is there any 43xx dev board that has the ULPI interface accessible so I can connect it to a second PHY or do I need to design&amp;nbsp;my own board to even get started on this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 04:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817665#M32739</guid>
      <dc:creator>eg0n</dc:creator>
      <dc:date>2018-06-27T04:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: USB1 ULPI interface on OM13088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817666#M32740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I think you'd better to design your own board.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 06:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-ULPI-interface-on-OM13088/m-p/817666#M32740</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-06-27T06:21:26Z</dc:date>
    </item>
  </channel>
</rss>