<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProblem when start location is not 0x00</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-when-start-location-is-not-0x00/m-p/817463#M32719</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with a LPC1317, which it contains an initial bootloader and application.&lt;/P&gt;&lt;P&gt;I am developing the Application, which I want to start it in 0x1000. I have configurated it (in MCUXpresso), and its size too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I try to debugg the App, there is not action. The Debugger ist not able to do anything. It is like the Debugger is not running from 0x1000 also from 0x00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any idea? I need to configurate anything more? I have looked for information, but I have only found the "Start Location" configuration in the MCU Settings, which I made.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Nov 2018 17:33:36 GMT</pubDate>
    <dc:creator>miguelbermejo</dc:creator>
    <dc:date>2018-11-08T17:33:36Z</dc:date>
    <item>
      <title>Problem when start location is not 0x00</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-when-start-location-is-not-0x00/m-p/817463#M32719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with a LPC1317, which it contains an initial bootloader and application.&lt;/P&gt;&lt;P&gt;I am developing the Application, which I want to start it in 0x1000. I have configurated it (in MCUXpresso), and its size too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I try to debugg the App, there is not action. The Debugger ist not able to do anything. It is like the Debugger is not running from 0x1000 also from 0x00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any idea? I need to configurate anything more? I have looked for information, but I have only found the "Start Location" configuration in the MCU Settings, which I made.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Nov 2018 17:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-when-start-location-is-not-0x00/m-p/817463#M32719</guid>
      <dc:creator>miguelbermejo</dc:creator>
      <dc:date>2018-11-08T17:33:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problem when start location is not 0x00</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-when-start-location-is-not-0x00/m-p/817464#M32720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application should be started&amp;nbsp;in 0x00. You cannot debug an application to&amp;nbsp;from 0x1000.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However,&amp;nbsp;you can use a&amp;nbsp; bootloader this will run from 0x00 and then jump to other address location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 21:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-when-start-location-is-not-0x00/m-p/817464#M32720</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-11-27T21:52:42Z</dc:date>
    </item>
  </channel>
</rss>