<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC2478 LCD clock</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478-LCD-clock/m-p/817175#M32712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Siva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a custom board, you should verify the general design recommendations for clock signals, as it seems to be hardware related (i.e. unbalanced impedances/capacitances).&lt;/P&gt;&lt;P&gt;As complementary information, you could take a look to the following links:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN10778.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN10778.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.onarm.com/forum/20290/"&gt;http://www.onarm.com/forum/20290/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Sep 2018 20:11:09 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-09-14T20:11:09Z</dc:date>
    <item>
      <title>LPC2478 LCD clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478-LCD-clock/m-p/817174#M32711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I have configured the LPC2478 LCDDCLK clock to 24MHz O/P and observed that the clock is not&amp;nbsp;reaching to full 0VDC on the negative transition.&lt;/P&gt;&lt;P&gt;I have made the following measurements and observe the issue:&lt;/P&gt;&lt;P&gt;1) Configured the DCLK at Pin 150 to 14MHz and observed the sine wave clk&amp;nbsp; with slow rise and fall times.&lt;/P&gt;&lt;P&gt;2) When it is configured to 24MHz clock the clock signal is not&amp;nbsp; reaching to complete 0VDC&amp;nbsp;&lt;SPAN&gt;on the negative transition.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please suggest the root&amp;nbsp;cause and possible trouble shooting techniques on this.Measurement WF are attached for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siva Bommaraju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 11:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478-LCD-clock/m-p/817174#M32711</guid>
      <dc:creator>sivaramakrishna</dc:creator>
      <dc:date>2018-09-12T11:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2478 LCD clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478-LCD-clock/m-p/817175#M32712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Siva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a custom board, you should verify the general design recommendations for clock signals, as it seems to be hardware related (i.e. unbalanced impedances/capacitances).&lt;/P&gt;&lt;P&gt;As complementary information, you could take a look to the following links:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN10778.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN10778.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.onarm.com/forum/20290/"&gt;http://www.onarm.com/forum/20290/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Sep 2018 20:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478-LCD-clock/m-p/817175#M32712</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-09-14T20:11:09Z</dc:date>
    </item>
  </channel>
</rss>