<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: build USB project, RAM using upto 50516byte, why? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816955#M32707</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Suggest you look in the linker map file to see what is using the space - I would guess it is used for buffers etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Aug 2018 09:04:27 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2018-08-04T09:04:27Z</dc:date>
    <item>
      <title>build USB project, RAM using upto 50516byte, why?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816952#M32704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. USB PROJECT:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; lpcopen_2_20\applications\lpc18xx_43xx\keil\keil_mcb_1857\lpcusblib_host\usbhost_msc\usbhost_msc&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Program Size: Code=27928 RO-data=1692 RW-data=108 ZI-data=48716 &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. but build SDcard file system using RAM following:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Program Size: Code=14770 RO-data=682 RW-data=48 ZI-data=6952 &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how do lessen RAM using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2018 02:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816952#M32704</guid>
      <dc:creator>9218sky</dc:creator>
      <dc:date>2018-08-03T02:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: build USB project, RAM using upto 50516byte, why?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816953#M32705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is optimization turned on? Try the -Os option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2018 13:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816953#M32705</guid>
      <dc:creator>chrispflieger</dc:creator>
      <dc:date>2018-08-03T13:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: build USB project, RAM using upto 50516byte, why?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816954#M32706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Chris&lt;/P&gt;&lt;P&gt;optimization&amp;nbsp;select&amp;nbsp;level-3, only code as lessen, but RAM no change!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Aug 2018 00:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816954#M32706</guid>
      <dc:creator>9218sky</dc:creator>
      <dc:date>2018-08-04T00:50:50Z</dc:date>
    </item>
    <item>
      <title>Re: build USB project, RAM using upto 50516byte, why?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816955#M32707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Suggest you look in the linker map file to see what is using the space - I would guess it is used for buffers etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Aug 2018 09:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816955#M32707</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2018-08-04T09:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: build USB project, RAM using upto 50516byte, why?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816956#M32708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Con Verse&lt;/P&gt;&lt;P&gt;look in map file, get&amp;nbsp;RAM expend information.&lt;/P&gt;&lt;P&gt;because "keil_startup_lpc18xx_43xx.s" define head size:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Heap_Size &amp;nbsp; &amp;nbsp; &amp;nbsp; EQU &amp;nbsp; &amp;nbsp; 0x00006000"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the value to 0Byte.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;build and test as successful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2018 14:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/build-USB-project-RAM-using-upto-50516byte-why/m-p/816956#M32708</guid>
      <dc:creator>9218sky</dc:creator>
      <dc:date>2018-08-06T14:09:12Z</dc:date>
    </item>
  </channel>
</rss>