<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 lpc11e68 SPI effective rate</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11e68-SPI-effective-rate/m-p/814342#M32659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using LPC11e68 system clock is set to 48MHz and&amp;nbsp;SSP0 configured as SPI master @ 12MHz.&lt;/P&gt;&lt;P&gt;it seems like effective baud rate is much lower - DMA is not in used and from the analysis i made it seems like reads/writes to SSP0 DR registers stalls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did anyone experience any similar performance issues with SPI?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i will appreciate any input.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Aug 2018 18:14:27 GMT</pubDate>
    <dc:creator>eranrai</dc:creator>
    <dc:date>2018-08-02T18:14:27Z</dc:date>
    <item>
      <title>lpc11e68 SPI effective rate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11e68-SPI-effective-rate/m-p/814342#M32659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using LPC11e68 system clock is set to 48MHz and&amp;nbsp;SSP0 configured as SPI master @ 12MHz.&lt;/P&gt;&lt;P&gt;it seems like effective baud rate is much lower - DMA is not in used and from the analysis i made it seems like reads/writes to SSP0 DR registers stalls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did anyone experience any similar performance issues with SPI?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i will appreciate any input.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2018 18:14:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11e68-SPI-effective-rate/m-p/814342#M32659</guid>
      <dc:creator>eranrai</dc:creator>
      <dc:date>2018-08-02T18:14:27Z</dc:date>
    </item>
    <item>
      <title>Re: lpc11e68 SPI effective rate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11e68-SPI-effective-rate/m-p/814343#M32660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If your SPI is set to 1/4 the CPU speed, you've only got 32 cycles for each byte. That's not much time for the CPU to do too much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2018 20:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11e68-SPI-effective-rate/m-p/814343#M32660</guid>
      <dc:creator>chrispflieger</dc:creator>
      <dc:date>2018-08-02T20:45:32Z</dc:date>
    </item>
  </channel>
</rss>