<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic usb  driver for windows10 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-driver-for-windows10/m-p/813326#M32631</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC2148&amp;nbsp;usb&amp;nbsp; driver for windows10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Nov 2018 05:32:40 GMT</pubDate>
    <dc:creator>1029124854</dc:creator>
    <dc:date>2018-11-29T05:32:40Z</dc:date>
    <item>
      <title>usb  driver for windows10</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-driver-for-windows10/m-p/813326#M32631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC2148&amp;nbsp;usb&amp;nbsp; driver for windows10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 05:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-driver-for-windows10/m-p/813326#M32631</guid>
      <dc:creator>1029124854</dc:creator>
      <dc:date>2018-11-29T05:32:40Z</dc:date>
    </item>
    <item>
      <title>Re: usb  driver for windows10</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-driver-for-windows10/m-p/813327#M32632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jackie,&lt;/P&gt;&lt;P&gt;The LPC21xx is part of the legacy devices and it has limited support. If you are referring to the USB drivers related to the debugger, you could contact to board manufacturer to ask of there is an updated version. Otherwise, you may consider using an external debugger with updated drivers, like Segger J-Link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you refer to custom USB drivers from a programmed USB application on the MCU, I’m afraid that we don’t have, although some of the generic USB drivers (like HID, MSD, CDC) are usually included on the newer operating system, just requiring some modification on the USB descriptors.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 21:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-driver-for-windows10/m-p/813327#M32632</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-12-04T21:28:47Z</dc:date>
    </item>
  </channel>
</rss>