<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic for LPC1769, is there a time delay needed when configuring SSP/SPI channels to transition between 16 and 8 bit transfer modes? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/for-LPC1769-is-there-a-time-delay-needed-when-configuring-SSP/m-p/812815#M32609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have 2 devices on the SSP0 but, one needs the usual 8 bit (byte) data transfers, but the other needs a 12 bit transfer (for which we configure SSP0 to send 16 bits). Since we talk to one device followed by talking to the other, we are constantly re-configuring. The device that used the 16 bits seems to be dropping data sometimes. When I inserted a delay before reconfigure to 16 bits, the data seems to have cleaned up. But the delay was 3 instructions. I wanted to find out if this is an issue and the proper way to address it is a delay.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any advice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Nov 2018 16:05:56 GMT</pubDate>
    <dc:creator>pgenerale</dc:creator>
    <dc:date>2018-11-07T16:05:56Z</dc:date>
    <item>
      <title>for LPC1769, is there a time delay needed when configuring SSP/SPI channels to transition between 16 and 8 bit transfer modes?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/for-LPC1769-is-there-a-time-delay-needed-when-configuring-SSP/m-p/812815#M32609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have 2 devices on the SSP0 but, one needs the usual 8 bit (byte) data transfers, but the other needs a 12 bit transfer (for which we configure SSP0 to send 16 bits). Since we talk to one device followed by talking to the other, we are constantly re-configuring. The device that used the 16 bits seems to be dropping data sometimes. When I inserted a delay before reconfigure to 16 bits, the data seems to have cleaned up. But the delay was 3 instructions. I wanted to find out if this is an issue and the proper way to address it is a delay.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any advice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2018 16:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/for-LPC1769-is-there-a-time-delay-needed-when-configuring-SSP/m-p/812815#M32609</guid>
      <dc:creator>pgenerale</dc:creator>
      <dc:date>2018-11-07T16:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: for LPC1769, is there a time delay needed when configuring SSP/SPI channels to transition between 16 and 8 bit transfer modes?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/for-LPC1769-is-there-a-time-delay-needed-when-configuring-SSP/m-p/812816#M32610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Piero Generale,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please share your code on how are making the re-configuration of the peripheral? Also, may I ask why are you sending 16 bits if the device needs 12 bit transfer? As you can see in the following table, you can select a data size of 12-bit. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74274i8130D44AFD2F354A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regard,&amp;nbsp; &lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2018 23:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/for-LPC1769-is-there-a-time-delay-needed-when-configuring-SSP/m-p/812816#M32610</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-11-09T23:06:25Z</dc:date>
    </item>
  </channel>
</rss>