<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Can't connect to SWD device after using BOARD_BootClockFROHF48M()</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812128#M32586</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jeremyzhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This method was successful to recover my MCU.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel Wetzel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Nov 2018 07:44:34 GMT</pubDate>
    <dc:creator>daniel_wetzel</dc:creator>
    <dc:date>2018-11-29T07:44:34Z</dc:date>
    <item>
      <title>Can't connect to SWD device after using BOARD_BootClockFROHF48M()</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812126#M32584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the OM13089 development board which includes the LPC54414.&lt;/P&gt;&lt;P&gt;After using the function&amp;nbsp;BOARD_BootClockFROHF48M() to change the frequency the debug process crashed and since that point I am not able to connect to the SWD device anymore.&lt;/P&gt;&lt;P&gt;The reason to why this occured is probably because I didn't use the function&amp;nbsp;CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH) before to enable the debug console to run with 12MHz.&lt;/P&gt;&lt;P&gt;But since the board won't allow the Link2 to connect to the SWD device anymore I don't know how to change the frequency back.&lt;/P&gt;&lt;P&gt;Is there any way to hard reset the board without using the Link2 connection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 10:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812126#M32584</guid>
      <dc:creator>daniel_wetzel</dc:creator>
      <dc:date>2018-11-28T10:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect to SWD device after using BOARD_BootClockFROHF48M()</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812127#M32585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="331259" data-username="daniel.wetzel@st.oth-regensburg.de" href="https://community.nxp.com/people/daniel.wetzel@st.oth-regensburg.de"&gt;Daniel Wetzel&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Whether the MCU becomes 'brick' now, if yes, I'd like to you to force the LPC54114 enter UART ISP mode, then erase the full flash area to recover the MCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78376iF2CB11706B5E1F64/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;You can learn how to use the Flash Magic connect with the LPC MCU via the below link.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://learn.adafruit.com/getting-started-with-the-lpc810/programming-the-lpc810-with-flash-magic" title="https://learn.adafruit.com/getting-started-with-the-lpc810/programming-the-lpc810-with-flash-magic"&gt;https://learn.adafruit.com/getting-started-with-the-lpc810/programming-the-lpc810-with-flash-magic&lt;/A&gt; &lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 02:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812127#M32585</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-11-29T02:32:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect to SWD device after using BOARD_BootClockFROHF48M()</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812128#M32586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jeremyzhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This method was successful to recover my MCU.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel Wetzel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 07:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-connect-to-SWD-device-after-using-BOARD-BootClockFROHF48M/m-p/812128#M32586</guid>
      <dc:creator>daniel_wetzel</dc:creator>
      <dc:date>2018-11-29T07:44:34Z</dc:date>
    </item>
  </channel>
</rss>