<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC845 HVQFN33 ADC won't provide correct counts</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/812087#M32582</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an LPCXpresso845MAX board. I am using ADC0 and ADC9 to acquire some signals. I started with the example code ADC_Seqa_Seqb and was able to get both channels to work. I have a desgined board that has the&amp;nbsp;HVQFN33&amp;nbsp; version of the chip on it. I can not seem to get the ADC to work with the same code as mentioned above. The ADC returns counts of about 15 on both channels when I should be getting counts on the order of 350. I know the board design works because I previously used it with an lpc824 (ADC0 and 9 worked fine in this case). The Xpresso845MAX board has the 64 pin chip on it. Is there something special I need to do for the&amp;nbsp;HVQFN33 chip? I have several builds of my board with the 845 on it and they are all behaving the same way.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Aug 2018 22:15:43 GMT</pubDate>
    <dc:creator>scottbates</dc:creator>
    <dc:date>2018-08-21T22:15:43Z</dc:date>
    <item>
      <title>LPC845 HVQFN33 ADC won't provide correct counts</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/812087#M32582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an LPCXpresso845MAX board. I am using ADC0 and ADC9 to acquire some signals. I started with the example code ADC_Seqa_Seqb and was able to get both channels to work. I have a desgined board that has the&amp;nbsp;HVQFN33&amp;nbsp; version of the chip on it. I can not seem to get the ADC to work with the same code as mentioned above. The ADC returns counts of about 15 on both channels when I should be getting counts on the order of 350. I know the board design works because I previously used it with an lpc824 (ADC0 and 9 worked fine in this case). The Xpresso845MAX board has the 64 pin chip on it. Is there something special I need to do for the&amp;nbsp;HVQFN33 chip? I have several builds of my board with the 845 on it and they are all behaving the same way.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 22:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/812087#M32582</guid>
      <dc:creator>scottbates</dc:creator>
      <dc:date>2018-08-21T22:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 HVQFN33 ADC won't provide correct counts</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/812088#M32583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott Bates,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;It seems a bit weird, the ADC is identical on all LPC845 parts, I was wondering if you can provide more information about this phenomenon, for instance, screenshots, etc.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 02:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/812088#M32583</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-08-22T02:50:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 HVQFN33 ADC won't provide correct counts</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/1189745#M43058</link>
      <description>&lt;P&gt;We are also facing the same problem&lt;/P&gt;&lt;P&gt;LPC845(HVQFN33) ADC is not Working&lt;/P&gt;&lt;P&gt;We downloaded SDK_2.8.0_LPC845 library for LPCXpresso845MAX and tested adc,adc functionality is working properly.&lt;BR /&gt;We designed board based on LPC845(HVQFN33) Package.We tested our board with the same library for adc application,we are not getting any adc value.(always showing adc count value as 12)&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 12:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-HVQFN33-ADC-won-t-provide-correct-counts/m-p/1189745#M43058</guid>
      <dc:creator>srchethan</dc:creator>
      <dc:date>2020-11-26T12:54:12Z</dc:date>
    </item>
  </channel>
</rss>