<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC54608 UART TX open drain or not?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-UART-TX-open-drain-or-not/m-p/808334#M32461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to use the pin named P0_30-ISP_FC0_TXD(A2)&amp;nbsp;as a&amp;nbsp;USART transmitter.&lt;/P&gt;&lt;P&gt;Is this pin an open drain pin by a default mode?&lt;/P&gt;&lt;P&gt;If this pin is an open drain pin, I have to put pull-up resistor.&lt;/P&gt;&lt;P&gt;I don't want to put pull-up resistor.&lt;/P&gt;&lt;P&gt;Please tell me whether pull-up resistor is needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the same way.&lt;BR /&gt;When also using D3,P12 pin as a USART transmitter, please tell me whether pull-up resistor is needed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Sep 2018 08:36:02 GMT</pubDate>
    <dc:creator>実奥山</dc:creator>
    <dc:date>2018-09-10T08:36:02Z</dc:date>
    <item>
      <title>LPC54608 UART TX open drain or not?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-UART-TX-open-drain-or-not/m-p/808334#M32461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to use the pin named P0_30-ISP_FC0_TXD(A2)&amp;nbsp;as a&amp;nbsp;USART transmitter.&lt;/P&gt;&lt;P&gt;Is this pin an open drain pin by a default mode?&lt;/P&gt;&lt;P&gt;If this pin is an open drain pin, I have to put pull-up resistor.&lt;/P&gt;&lt;P&gt;I don't want to put pull-up resistor.&lt;/P&gt;&lt;P&gt;Please tell me whether pull-up resistor is needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the same way.&lt;BR /&gt;When also using D3,P12 pin as a USART transmitter, please tell me whether pull-up resistor is needed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2018 08:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-UART-TX-open-drain-or-not/m-p/808334#M32461</guid>
      <dc:creator>実奥山</dc:creator>
      <dc:date>2018-09-10T08:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 UART TX open drain or not?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-UART-TX-open-drain-or-not/m-p/808335#M32462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is a stardard I/O pin.The default configuration for standard I/O pins is Z mode. The weak MOS devices provide a drive capability equivalent to pull-up and pull-down resistors.&lt;/P&gt;&lt;P&gt;The below figure shows the possible pin modes for standard I/O pins:&lt;/P&gt;&lt;P&gt;• Digital output driver: enabled/disabled.&lt;/P&gt;&lt;P&gt;• Digital input: Pull-up enabled/disabled.&lt;/P&gt;&lt;P&gt;• Digital input: Pull-down enabled/disabled.&lt;/P&gt;&lt;P&gt;• Digital input: Repeater mode enabled/disabled.&lt;/P&gt;&lt;P&gt;• Z mode; High impedance (no cross-bar currents for floating inputs).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68560i95BEFBD60889C372/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2018 16:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-UART-TX-open-drain-or-not/m-p/808335#M32462</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-09-10T16:55:19Z</dc:date>
    </item>
  </channel>
</rss>