<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Controlling via an app?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803990#M32299</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply, unfortunately I thought that might be the situation!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Sep 2018 20:06:07 GMT</pubDate>
    <dc:creator>leo838</dc:creator>
    <dc:date>2018-09-28T20:06:07Z</dc:date>
    <item>
      <title>Controlling via an app?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803988#M32297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;Just wondering if anyone has implemented a efficient way of communicating/controlling an LPC from an app on a mobile device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm implementing a home ventilation system controlled by a 1769 &amp;amp; ideally would like to be control it via an app. I think a webserver would be overkill &amp;amp; I don't want to compromise the control of the ventilation system (which uses ac waveform cutting with a triac).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at &lt;A href="https://community.nxp.com/www.blynk.cc" target="test_blank"&gt;www.blynk.cc&lt;/A&gt; but it doesn't have anything for an LPC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone recommend a way/ solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 19:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803988#M32297</guid>
      <dc:creator>leo838</dc:creator>
      <dc:date>2018-09-27T19:13:15Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling via an app?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803989#M32298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo838,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to use the LPC to be controlled by the mobile app.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I think, just the LPC1769 chip is not enough, you may can associated with the WIFI chip, then the mobile app can control it through the wifi web. Or, you can use the Ethernet network, then you need to connect your mobile app to the website, through the website to control the LPC1769.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This is the method, we still don't have the according application for your reference, so you need to design it by yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 09:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803989#M32298</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-28T09:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling via an app?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803990#M32299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply, unfortunately I thought that might be the situation!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 20:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803990#M32299</guid>
      <dc:creator>leo838</dc:creator>
      <dc:date>2018-09-28T20:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling via an app?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803991#M32300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can try it, if when you do it in details, and meet the problem, just let us know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2018 07:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803991#M32300</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-29T07:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling via an app?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803992#M32301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you looked at ARM's Mbed? This offers a lot of web integration. Mbed was originally exclusive to LPC parts, and&amp;nbsp;has now expanded considerably, but they are still well supported&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.mbed.com" target="test_blank"&gt;www.mbed.com&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2018 08:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803992#M32301</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2018-09-29T08:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling via an app?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803993#M32302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the suggestion, I'll take a look&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Oct 2018 19:43:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Controlling-via-an-app/m-p/803993#M32302</guid>
      <dc:creator>leo838</dc:creator>
      <dc:date>2018-10-06T19:43:55Z</dc:date>
    </item>
  </channel>
</rss>