<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1768 UART Receive Enable</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802869#M32263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Victor for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess, the data will be received and stored into RX FIFO even though RX interrupts are deactivated. So I would try option 2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Aug 2018 19:40:10 GMT</pubDate>
    <dc:creator>marysoniadurom</dc:creator>
    <dc:date>2018-08-22T19:40:10Z</dc:date>
    <item>
      <title>LPC1768 UART Receive Enable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802867#M32261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any options to enable/disable Reception in LPC1768 UART?.&lt;/P&gt;&lt;P&gt;In the User Manual UM10360, it is stated that TXEN in UxTER register can be used to enable/disable Transmission.&amp;nbsp; But could not able to find anything similar for Reception.&lt;/P&gt;&lt;P&gt;My application code requires to stop receiving unwanted data some times and to stop receiving while transmitting. How this can be possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 13:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802867#M32261</guid>
      <dc:creator>marysoniadurom</dc:creator>
      <dc:date>2018-08-20T13:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART Receive Enable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802868#M32262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Mary Durom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you have two different options:&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;You can deactivate all the interrupts involved with Rx when you don't want to receive any information.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;You can change the function of the UART Rx pin when you don't want to receive information, for example to the GPIO function.&amp;nbsp;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 21:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802868#M32262</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-08-21T21:26:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART Receive Enable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802869#M32263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Victor for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess, the data will be received and stored into RX FIFO even though RX interrupts are deactivated. So I would try option 2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 19:40:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-Receive-Enable/m-p/802869#M32263</guid>
      <dc:creator>marysoniadurom</dc:creator>
      <dc:date>2018-08-22T19:40:10Z</dc:date>
    </item>
  </channel>
</rss>