<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC5460x without  oscillator input (XTALIN) possible? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798325#M32120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Liang,&lt;/P&gt;&lt;P&gt;I do NOT have a RTC xtal mounted and I do also NOT use the RTC, so can't help you.&lt;/P&gt;&lt;P&gt;But, I would think that the RTC will NOT work without the RTC xtal, most NXP processors I use require the RTC xtal if you are going to use RTC. I would expect the same for the 546x series, but need to check with others.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Nov 2018 12:47:19 GMT</pubDate>
    <dc:creator>carstengroen</dc:creator>
    <dc:date>2018-11-05T12:47:19Z</dc:date>
    <item>
      <title>LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798320#M32115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; From the datasheet, I can generate 180M system clock from FRO_12M clock or CLK_IN(see attached).&lt;/P&gt;&lt;P&gt;but in datasheet page 53 table 5(attached below), says:&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="155"&gt;&lt;SPAN class=""&gt;XTALIN&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD width="55"&gt;&lt;SPAN class=""&gt;-&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD width="448"&gt;&lt;SPAN class=""&gt;Connect to ground. When grounded, the RTC oscillator is disabled.&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Does this mean, I can't run 5460x with out oscillator input? I just want to simplify the design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19409i0756EC9932234D38/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19500i9F0E178455AFE7E1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 00:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798320#M32115</guid>
      <dc:creator>topkinschen</dc:creator>
      <dc:date>2018-11-05T00:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798321#M32116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can run the CPU without external xtal (I use the 12 MHz internal to generate 180 MHz clock)&lt;/P&gt;&lt;P&gt;You need to check requirements if using USB (high/full speed etc)!!&lt;/P&gt;&lt;P&gt;The text in the datasheet is wrong, it says ("Connect to ground. When grounded, the RTC OSCILLATOR is disabled")&lt;/P&gt;&lt;P&gt;This is clearly a typical "cut&amp;amp;paste" error from the RTCXIN pin description :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 08:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798321#M32116</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2018-11-05T08:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798322#M32117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;STRONG class=""&gt;&lt;SPAN class=""&gt;Carsten &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I don't use USB, and I just want to double check with you: you don't use external xtal, and your RTC works fine,&amp;nbsp; is that right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 08:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798322#M32117</guid>
      <dc:creator>topkinschen</dc:creator>
      <dc:date>2018-11-05T08:43:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798323#M32118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry Liang,&lt;/P&gt;&lt;P&gt;I was not&amp;nbsp;aware that&amp;nbsp;you meant the RTC and not the normal CPU clock!&lt;/P&gt;&lt;P&gt;In case of the RTC, I don't know, but I would assume that an external xtal is needed for it to work (several of NXPs other processors does need external RTC xtal for the RTC to work)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 08:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798323#M32118</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2018-11-05T08:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798324#M32119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;Carsten&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I don't make it clear, Sorry for misunderstanding.&lt;/P&gt;&lt;P&gt;what I just want to say is :you don't use external xtal for MCU main clock(of course you use 32k&amp;nbsp;&lt;SPAN class=""&gt; RTC oscillator&lt;/SPAN&gt; as normal ),&amp;nbsp; and your RTC works fine,&amp;nbsp; is that right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I just want to double check the datasheet about this should say"&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="155"&gt;&lt;SPAN class=""&gt;XTALIN&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD width="55"&gt;&lt;SPAN class=""&gt;-&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD width="448"&gt;&lt;SPAN class=""&gt;Connect to ground. When grounded, the&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt; XTAL&lt;/STRONG&gt;&lt;/SPAN&gt; oscillator is disabled.&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 09:06:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798324#M32119</guid>
      <dc:creator>topkinschen</dc:creator>
      <dc:date>2018-11-05T09:06:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798325#M32120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Liang,&lt;/P&gt;&lt;P&gt;I do NOT have a RTC xtal mounted and I do also NOT use the RTC, so can't help you.&lt;/P&gt;&lt;P&gt;But, I would think that the RTC will NOT work without the RTC xtal, most NXP processors I use require the RTC xtal if you are going to use RTC. I would expect the same for the 546x series, but need to check with others.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 12:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798325#M32120</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2018-11-05T12:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798326#M32121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can run the CPU without external xtal like Carsten mentioned, if you don't need the RTC the RTC xtal it is not necessary.&amp;nbsp; If you need the RTC you need to put the RTC xtal.&lt;/P&gt;&lt;P style="border: 0px; font-size: 14px;"&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P style="border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="border: 0px; font-size: 14px;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 20:14:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798326#M32121</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-11-05T20:14:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798327#M32122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; From the datasheet, &lt;STRONG&gt;if &lt;SPAN class=""&gt;XTALIN&lt;/SPAN&gt; is not connected and grounded then RTC is &lt;SPAN class=""&gt;disabled, &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN class=""&gt;that means if I don't mount XTALIN, RTC will not work whether or not RTCXIN is mounted.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I just want to double check:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if the datasheet make a "copy&amp;amp;paste" mistake as &lt;STRONG class=""&gt;Carsten &lt;/STRONG&gt;say. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OR, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; datasheet is correct, it's designed behavior?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62093i5DFDB077E97F089B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 01:03:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798327#M32122</guid>
      <dc:creator>topkinschen</dc:creator>
      <dc:date>2018-11-06T01:03:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5460x without  oscillator input (XTALIN) possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798328#M32123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, this is a mistake as Carten say. I will inform to our documentation team.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your feedback&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Sol&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 15:25:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5460x-without-oscillator-input-XTALIN-possible/m-p/798328#M32123</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-11-06T15:25:40Z</dc:date>
    </item>
  </channel>
</rss>