<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe:  lpc540xx XIP</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc540xx-XIP/m-p/797987#M32097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Avi Makmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please provide more information of which LPC are you using?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look into the following application note:&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12122.pdf" title="https://www.nxp.com/docs/en/application-note/AN12122.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12122.pdf&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Which explains how to modify the header structure of the image in order to&amp;nbsp;run code from the external flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2018 19:54:33 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2018-07-12T19:54:33Z</dc:date>
    <item>
      <title>lpc540xx XIP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc540xx-XIP/m-p/797986#M32096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Where can i find the code which do XIP (Execution In Place) from external SPI flash (Micron), in the SDK there is Download image XIP example, but I need to run code from the external flash in XIP,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks In advance&lt;/P&gt;&lt;P&gt;Avi Makmal&lt;/P&gt;&lt;P&gt;WINBOND&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2018 14:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc540xx-XIP/m-p/797986#M32096</guid>
      <dc:creator>amakmal</dc:creator>
      <dc:date>2018-07-10T14:15:04Z</dc:date>
    </item>
    <item>
      <title>Re:  lpc540xx XIP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc540xx-XIP/m-p/797987#M32097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Avi Makmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please provide more information of which LPC are you using?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look into the following application note:&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12122.pdf" title="https://www.nxp.com/docs/en/application-note/AN12122.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12122.pdf&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Which explains how to modify the header structure of the image in order to&amp;nbsp;run code from the external flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 19:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc540xx-XIP/m-p/797987#M32097</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-07-12T19:54:33Z</dc:date>
    </item>
  </channel>
</rss>