<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How can I attach an I2C device to the Arduino bus on the LPCXpresso54628 board? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-attach-an-I2C-device-to-the-Arduino-bus-on-the/m-p/796577#M32055</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Greg,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend&amp;nbsp;you to download the newest version of the SDK (2.4.1). Within the SDK you will find multiple examples of I2C applications. You can use this as a guide to see how to make all the configurations. For example, the project&amp;nbsp;&lt;EM&gt;lpcxpresso54628_i2c_interrupt_b2b_transfer_master&lt;/EM&gt; configures pins P1_17 and P1_18 to work in I2C master mode. These pins are from the Arduino&amp;nbsp;shield, but they use Flexcomm8, is there any particular reason you want to use Flexcomm3?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;Link to download the SDK.&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2018 17:05:13 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2018-09-27T17:05:13Z</dc:date>
    <item>
      <title>How can I attach an I2C device to the Arduino bus on the LPCXpresso54628 board?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-attach-an-I2C-device-to-the-Arduino-bus-on-the/m-p/796576#M32054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use a different LCD screen with the development board.&amp;nbsp; This one use the standard 4 pin connector for its touch function (+X, +Y, -X, -Y), but I have an adapter which converts that to an I2C input.&amp;nbsp; I tried using the PMOD connector to attach it, but am running into conflicts with the Linkserver connection for the probe.&amp;nbsp; So, I would like to use Flexcomm3, which is (If I'm reading this correctly) part of the Arduino bus.&amp;nbsp; How can I use Flexcomm3 for this device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 14:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-attach-an-I2C-device-to-the-Arduino-bus-on-the/m-p/796576#M32054</guid>
      <dc:creator>greg_smith</dc:creator>
      <dc:date>2018-09-25T14:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: How can I attach an I2C device to the Arduino bus on the LPCXpresso54628 board?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-attach-an-I2C-device-to-the-Arduino-bus-on-the/m-p/796577#M32055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Greg,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend&amp;nbsp;you to download the newest version of the SDK (2.4.1). Within the SDK you will find multiple examples of I2C applications. You can use this as a guide to see how to make all the configurations. For example, the project&amp;nbsp;&lt;EM&gt;lpcxpresso54628_i2c_interrupt_b2b_transfer_master&lt;/EM&gt; configures pins P1_17 and P1_18 to work in I2C master mode. These pins are from the Arduino&amp;nbsp;shield, but they use Flexcomm8, is there any particular reason you want to use Flexcomm3?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;Link to download the SDK.&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 17:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-attach-an-I2C-device-to-the-Arduino-bus-on-the/m-p/796577#M32055</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-27T17:05:13Z</dc:date>
    </item>
  </channel>
</rss>