<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is it possible to write data on EMC flash where code is running in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-write-data-on-EMC-flash-where-code-is-running/m-p/796037#M32034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Priyank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I understood correct, you want to write in the flash while you are executing also from flash, right?&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is not possible, if you want to write in flash then you must be running from RAM. For example, you should move the specific functions that are writing on the flash to the RAM memory. I recommend you read the following community post to see how to do this.&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-335283"&gt;Relocating Code and Data Using the MCUXpresso IDE&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2018 19:08:18 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2018-09-06T19:08:18Z</dc:date>
    <item>
      <title>Is it possible to write data on EMC flash where code is running</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-write-data-on-EMC-flash-where-code-is-running/m-p/796036#M32033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I am facing a problem regarding EMC Nor flash SST39VF3201C. I have my bootloader code on internal flash &amp;amp; user application on EMC nor flash. But when I try to write some data(variables) using LPCOpen APIs on a specific address far from code address it causes hard fault. I have initialized flash in bootloader &amp;amp; not(again) in user application. Code works fine &amp;amp; reading from an address is working too. Is there any solution for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Priyank.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 13:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-write-data-on-EMC-flash-where-code-is-running/m-p/796036#M32033</guid>
      <dc:creator>priyankb</dc:creator>
      <dc:date>2018-09-05T13:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to write data on EMC flash where code is running</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-write-data-on-EMC-flash-where-code-is-running/m-p/796037#M32034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Priyank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I understood correct, you want to write in the flash while you are executing also from flash, right?&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is not possible, if you want to write in flash then you must be running from RAM. For example, you should move the specific functions that are writing on the flash to the RAM memory. I recommend you read the following community post to see how to do this.&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-335283"&gt;Relocating Code and Data Using the MCUXpresso IDE&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 19:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-write-data-on-EMC-flash-where-code-is-running/m-p/796037#M32034</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-06T19:08:18Z</dc:date>
    </item>
  </channel>
</rss>