<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4357JET256 nRESET doesn't work in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792840#M31906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Don't see a lot of reasons for such an issue, both devices are the same silicon version 'A', one produced in week 02/2015 and the other one in week 16/2017.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you maybe read out the Boot ROM version on both devices?&lt;/P&gt;&lt;P&gt;Is it just one new device where it doesn't work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Sep 2018 13:24:26 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2018-09-26T13:24:26Z</dc:date>
    <item>
      <title>LPC4357JET256 nRESET doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792839#M31905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know what is change in the two different version below ? Somehow I can't get the "nRESET" work in a newer version, but the older version working fine. Every time I press manual reset then the MCU hanging. Thank you for help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Newer&amp;nbsp;Version:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;-LPC4357JET256&lt;/P&gt;&lt;P&gt;-&lt;STRONG&gt;PBFV15.00&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-ESD17160a&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Older Version:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;-LPC4357JET256&lt;/P&gt;&lt;P&gt;-&lt;STRONG&gt;PIXN23.00&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-ESD15020A&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 22:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792839#M31905</guid>
      <dc:creator>mike_phan</dc:creator>
      <dc:date>2018-09-25T22:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357JET256 nRESET doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792840#M31906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Don't see a lot of reasons for such an issue, both devices are the same silicon version 'A', one produced in week 02/2015 and the other one in week 16/2017.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you maybe read out the Boot ROM version on both devices?&lt;/P&gt;&lt;P&gt;Is it just one new device where it doesn't work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 13:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792840#M31906</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2018-09-26T13:24:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357JET256 nRESET doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792841#M31907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Bernard.&lt;/P&gt;&lt;P&gt;Can you show me how do you read out the Boot ROM version?&lt;/P&gt;&lt;P&gt;it happens to all chips with new date code &lt;STRONG&gt;ESD17160A.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 18:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792841#M31907</guid>
      <dc:creator>mike_phan</dc:creator>
      <dc:date>2018-09-26T18:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357JET256 nRESET doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792842#M31908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="327121" data-username="mike.phan@ga.com" href="https://community.nxp.com/people/mike.phan@ga.com"&gt;mike phan&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;Flash Magic tool is able to read out the Boot ROM version when connecting the LPC4357 which is forced to enter ISP mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71013i4DF380F6FD179D07/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;You can learn how to do it via the following link.&lt;BR /&gt;&lt;A href="https://learn.adafruit.com/getting-started-with-the-lpc810/programming-the-lpc810-with-flash-magic"&gt;https://learn.adafruit.com/getting-started-with-the-lpc810/programming-the-lpc810-with-flash-magic&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 01:54:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792842#M31908</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-09-27T01:54:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357JET256 nRESET doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792843#M31909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the rerason why I'm asking for the ROM version:&amp;nbsp; there is a problem like this under certain conditions on the old silicon version which is marked with '-'. See in this thread:&amp;nbsp; &lt;A href="https://community.nxp.com/thread/442014"&gt;LPC1857- Revision changes 'A' vs '-'- Impact on sleep and reset.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;This is a known bug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that the marking goes in line with the right silicon version in the package, but I can't exclude it.&lt;/P&gt;&lt;P&gt;So by reading the same ROM version number from both chips you mentioned, you would make sure that it is the same silicon and therefore we need to investigate in a different direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 09:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357JET256-nRESET-doesn-t-work/m-p/792843#M31909</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2018-09-27T09:20:19Z</dc:date>
    </item>
  </channel>
</rss>