<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC1769 Flashing issue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791309#M31872</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an issue for download the image:&lt;BR /&gt;02:failed to connect: Ep(0). target marked as not debugabble&lt;BR /&gt;i tried already all the possible solution for it in the related topics in the below link :&lt;BR /&gt;1-&lt;A href="https://community.nxp.com/thread/389112"&gt;Regaining debug access to target MCU&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;but it is not solved the problem&lt;BR /&gt;&lt;STRONG&gt;that is the log from the flashing :&lt;BR /&gt;&lt;/STRONG&gt;&lt;BR /&gt;Nc: Serial Number: HID64HS12&lt;BR /&gt;Nc: VID:PID: 1FC9:0007&lt;BR /&gt;Nc: USB Path: &lt;BR /&gt;Nc: CM3/4 debug bus (DP 0x2BA01477 MemAP[0] 0x04770011) SWD connection failed - 'Nn(05). ACK Fault'&lt;BR /&gt;Nc: connection failed - Ep(01). Target marked as not debuggable. - retrying&lt;BR /&gt;Nc: non-Cortex debug bus (DP 0xFFFFFFFF MemAP[0] 0x04770001) SWD connection failed - 'Nn(05). ACK Fault'&lt;BR /&gt;Wc: Vector catch on VECTRESET signal&lt;BR /&gt;Nc: Debug bus check after stop (MemAP 0x4770001) FAILS - Em(02). MEM-AP is not selected.&lt;BR /&gt;Ed:02: Failed on connect: Ep(01). Target marked as not debuggable.&lt;BR /&gt;Et: Emu(0): Connected&amp;amp;Reset. Was: NotConnected. DpID: 00000000. CpuID: 00000000. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Nc: Last stub error 0: OK&lt;BR /&gt;Nc: Last sticky error: 0x0 AIndex: 0&lt;BR /&gt;Nc: No debug bus (MemAp) selected&lt;BR /&gt;Nc: DAP Speed test unexecuted or failed&lt;BR /&gt;Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Pc: (100) Target Connection Failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any one could help me ?&lt;BR /&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Oct 2018 20:45:03 GMT</pubDate>
    <dc:creator>ibrahim_elaasy</dc:creator>
    <dc:date>2018-10-31T20:45:03Z</dc:date>
    <item>
      <title>LPC1769 Flashing issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791309#M31872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an issue for download the image:&lt;BR /&gt;02:failed to connect: Ep(0). target marked as not debugabble&lt;BR /&gt;i tried already all the possible solution for it in the related topics in the below link :&lt;BR /&gt;1-&lt;A href="https://community.nxp.com/thread/389112"&gt;Regaining debug access to target MCU&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;but it is not solved the problem&lt;BR /&gt;&lt;STRONG&gt;that is the log from the flashing :&lt;BR /&gt;&lt;/STRONG&gt;&lt;BR /&gt;Nc: Serial Number: HID64HS12&lt;BR /&gt;Nc: VID:PID: 1FC9:0007&lt;BR /&gt;Nc: USB Path: &lt;BR /&gt;Nc: CM3/4 debug bus (DP 0x2BA01477 MemAP[0] 0x04770011) SWD connection failed - 'Nn(05). ACK Fault'&lt;BR /&gt;Nc: connection failed - Ep(01). Target marked as not debuggable. - retrying&lt;BR /&gt;Nc: non-Cortex debug bus (DP 0xFFFFFFFF MemAP[0] 0x04770001) SWD connection failed - 'Nn(05). ACK Fault'&lt;BR /&gt;Wc: Vector catch on VECTRESET signal&lt;BR /&gt;Nc: Debug bus check after stop (MemAP 0x4770001) FAILS - Em(02). MEM-AP is not selected.&lt;BR /&gt;Ed:02: Failed on connect: Ep(01). Target marked as not debuggable.&lt;BR /&gt;Et: Emu(0): Connected&amp;amp;Reset. Was: NotConnected. DpID: 00000000. CpuID: 00000000. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Nc: Last stub error 0: OK&lt;BR /&gt;Nc: Last sticky error: 0x0 AIndex: 0&lt;BR /&gt;Nc: No debug bus (MemAp) selected&lt;BR /&gt;Nc: DAP Speed test unexecuted or failed&lt;BR /&gt;Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Pc: (100) Target Connection Failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any one could help me ?&lt;BR /&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 20:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791309#M31872</guid>
      <dc:creator>ibrahim_elaasy</dc:creator>
      <dc:date>2018-10-31T20:45:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 Flashing issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791310#M31873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Maybe you should consider this issue is related to the hardware, so I was wondering if you can introduce which board and demo code you use for the testing.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 01:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791310#M31873</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-11-01T01:52:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 Flashing issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791311#M31874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board is LPC 1769 connected it to LPCxpresso IDE through USB , i tried first to flash a program that make led blinks and give me that message while flashing "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;02:failed to connect: Ep(0). target marked as not debugabble&lt;/SPAN&gt;" .&lt;BR /&gt;Then i tried a simple program&amp;nbsp; &amp;nbsp;While(1){i++;}&amp;nbsp; . and still the the same message exist .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 09:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791311#M31874</guid>
      <dc:creator>ibrahim_elaasy</dc:creator>
      <dc:date>2018-11-01T09:27:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 Flashing issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791312#M31875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;Whether your board is OM13085 (LPCXpreeso 1769 board), if not, I was wondering if you can share the schematic of the board and I can review it for you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Nov 2018 02:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-Flashing-issue/m-p/791312#M31875</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-11-02T02:13:14Z</dc:date>
    </item>
  </channel>
</rss>