<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Debug problem with my new LPC 54018 IoT Module OM40006 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Debug-problem-with-my-new-LPC-54018-IoT-Module-OM40006/m-p/789506#M31771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on NXP OM40006 IoT Module Baseboard (LPC 54018). I'm using MCUXpresso IDE with the respective SDK installed.&amp;nbsp; I've tried to run the Hello World program from the demo apps of the installed SDK and I keep on getting this error attached in the screenshot when I try to debug the program.&amp;nbsp;I need help in understanding this error. I've set the jumper configurations as per given in the user manual of the board. I've tried following steps which didn't solve my problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Power recycling the board.&lt;/P&gt;&lt;P&gt;2. Changing the USB Ports.&lt;/P&gt;&lt;P&gt;3. Using multiple cables.&lt;/P&gt;&lt;P&gt;4. Also tried debugging using Segger J-Link which was of no use.&lt;/P&gt;&lt;P&gt;5. Tried using multiple PCs (Windows 10).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is the screenshot of the error. Please help me in resolving this issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Saranya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Sep 2018 22:28:55 GMT</pubDate>
    <dc:creator>saranyachitta</dc:creator>
    <dc:date>2018-09-23T22:28:55Z</dc:date>
    <item>
      <title>Debug problem with my new LPC 54018 IoT Module OM40006</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Debug-problem-with-my-new-LPC-54018-IoT-Module-OM40006/m-p/789506#M31771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on NXP OM40006 IoT Module Baseboard (LPC 54018). I'm using MCUXpresso IDE with the respective SDK installed.&amp;nbsp; I've tried to run the Hello World program from the demo apps of the installed SDK and I keep on getting this error attached in the screenshot when I try to debug the program.&amp;nbsp;I need help in understanding this error. I've set the jumper configurations as per given in the user manual of the board. I've tried following steps which didn't solve my problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Power recycling the board.&lt;/P&gt;&lt;P&gt;2. Changing the USB Ports.&lt;/P&gt;&lt;P&gt;3. Using multiple cables.&lt;/P&gt;&lt;P&gt;4. Also tried debugging using Segger J-Link which was of no use.&lt;/P&gt;&lt;P&gt;5. Tried using multiple PCs (Windows 10).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is the screenshot of the error. Please help me in resolving this issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Saranya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Sep 2018 22:28:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Debug-problem-with-my-new-LPC-54018-IoT-Module-OM40006/m-p/789506#M31771</guid>
      <dc:creator>saranyachitta</dc:creator>
      <dc:date>2018-09-23T22:28:55Z</dc:date>
    </item>
    <item>
      <title>Re: Debug problem with my new LPC 54018 IoT Module OM40006</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Debug-problem-with-my-new-LPC-54018-IoT-Module-OM40006/m-p/789507#M31772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Saranya,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please be sure that you are connecting right the&amp;nbsp;OM40007: LPC54018 IoT Module into the IoT Module base board, as shown in the following image.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IoT module.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69658iADD3ED27F632418A/image-size/large?v=v2&amp;amp;px=999" role="button" title="IoT module.jpg" alt="IoT module.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 16:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Debug-problem-with-my-new-LPC-54018-IoT-Module-OM40006/m-p/789507#M31772</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-25T16:57:21Z</dc:date>
    </item>
  </channel>
</rss>