<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The Initial Status of LPC11C24 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-Initial-Status-of-LPC11C24/m-p/787443#M31666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rasheed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCUs come with a blank FLASH memory from the factory but please notice that the LPC11C24 MCUs have also a ROM memory with a bootloader that controls initial operation after reset and also provides the means to accomplish programming of the flash memory via UART or C_CAN.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2018 21:42:23 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2018-11-21T21:42:23Z</dc:date>
    <item>
      <title>The Initial Status of LPC11C24</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-Initial-Status-of-LPC11C24/m-p/787442#M31665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;When we buy a new a single chip LPC11C24, what is the status of its flash memory???&lt;/P&gt;&lt;P&gt;1. without boatloader??? In this case how can I flash it??&lt;/P&gt;&lt;P&gt;2. Or with booatloader???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Rasheed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 14:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-Initial-Status-of-LPC11C24/m-p/787442#M31665</guid>
      <dc:creator>rasheedkhankan</dc:creator>
      <dc:date>2018-11-21T14:18:02Z</dc:date>
    </item>
    <item>
      <title>Re: The Initial Status of LPC11C24</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-Initial-Status-of-LPC11C24/m-p/787443#M31666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rasheed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCUs come with a blank FLASH memory from the factory but please notice that the LPC11C24 MCUs have also a ROM memory with a bootloader that controls initial operation after reset and also provides the means to accomplish programming of the flash memory via UART or C_CAN.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 21:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-Initial-Status-of-LPC11C24/m-p/787443#M31666</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-11-21T21:42:23Z</dc:date>
    </item>
  </channel>
</rss>