<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CANopen in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CANopen/m-p/787015#M31653</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunatelly, not all features of CANopen are implemented in the demo, but the most-used features of CANopen are supported:&lt;BR /&gt;• SDO expedited transfer: client &amp;amp; server.&lt;BR /&gt;• SDO segmented transfer: client &amp;amp; server.&lt;BR /&gt;• NMT: master, slave &amp;amp; boot-up.&lt;BR /&gt;• Heartbeat: producer &amp;amp; consumer.&lt;BR /&gt;The demo will demonstrate these features with the aid of a terminal program and the onboard LEDs and buttons.&lt;/P&gt;&lt;P&gt;PDO transfer, synchronization, time stamp and emergency are not realized in the demo, you have to implement PDO yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest to check the guidelines showed in this post:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://stackoverflow.com/questions/28038585/canopen-pdo-sample-code-for-lpc11cxx" title="https://stackoverflow.com/questions/28038585/canopen-pdo-sample-code-for-lpc11cxx"&gt;CANopen PDO sample code for LPC11Cxx - Stack Overflow&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Aug 2018 15:50:55 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2018-08-14T15:50:55Z</dc:date>
    <item>
      <title>CANopen</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CANopen/m-p/787014#M31652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone has any simple example of CANopen implementation (especialy PDO usage)? I found AN11238_1 demo, but there isn't any example or api about PDO. I practice SDO tx and rx with the LPC11Cxx demo and read on internet documentation about PDO, but this was not enough for me to implement PDO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 12:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CANopen/m-p/787014#M31652</guid>
      <dc:creator>inseparatio</dc:creator>
      <dc:date>2018-08-14T12:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: CANopen</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CANopen/m-p/787015#M31653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunatelly, not all features of CANopen are implemented in the demo, but the most-used features of CANopen are supported:&lt;BR /&gt;• SDO expedited transfer: client &amp;amp; server.&lt;BR /&gt;• SDO segmented transfer: client &amp;amp; server.&lt;BR /&gt;• NMT: master, slave &amp;amp; boot-up.&lt;BR /&gt;• Heartbeat: producer &amp;amp; consumer.&lt;BR /&gt;The demo will demonstrate these features with the aid of a terminal program and the onboard LEDs and buttons.&lt;/P&gt;&lt;P&gt;PDO transfer, synchronization, time stamp and emergency are not realized in the demo, you have to implement PDO yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest to check the guidelines showed in this post:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://stackoverflow.com/questions/28038585/canopen-pdo-sample-code-for-lpc11cxx" title="https://stackoverflow.com/questions/28038585/canopen-pdo-sample-code-for-lpc11cxx"&gt;CANopen PDO sample code for LPC11Cxx - Stack Overflow&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 15:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CANopen/m-p/787015#M31653</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-08-14T15:50:55Z</dc:date>
    </item>
  </channel>
</rss>