<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1758 using RMII to connect switch chip in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786276#M31611</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue may refer to memory locations, please check the below thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/426813"&gt;LPC1788 Ethernet DMA interrupt problem&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2018 15:03:46 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2018-09-06T15:03:46Z</dc:date>
    <item>
      <title>LPC1758 using RMII to connect switch chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786275#M31610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using LPC1758 to connect a four port switch (using RMII, mac to phy). I already configured EMAC module and can see frames are sent out from switch ports. It seems Tx in LPC1758 EMAC is working. But Rx is not working. I print the&amp;nbsp; two Rx registers:&amp;nbsp;RxProduceIndex and&amp;nbsp;RxConsumeIndex. Both of them are always zero. Is that any special config will cause Tx works but Rx not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Sep 2018 08:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786275#M31610</guid>
      <dc:creator>sonic_hsieh</dc:creator>
      <dc:date>2018-09-03T08:22:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1758 using RMII to connect switch chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786276#M31611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue may refer to memory locations, please check the below thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/426813"&gt;LPC1788 Ethernet DMA interrupt problem&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 15:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786276#M31611</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-09-06T15:03:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1758 using RMII to connect switch chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786277#M31612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I think problem is solved. I find RMII RX_DV is wrong connected to other pin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Fixed it and RMII Tx/Rx are working normally now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Thanks the support.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 01:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-using-RMII-to-connect-switch-chip/m-p/786277#M31612</guid>
      <dc:creator>sonic_hsieh</dc:creator>
      <dc:date>2018-09-12T01:47:59Z</dc:date>
    </item>
  </channel>
</rss>