<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54018 IoT with SPIFI code in XIP bricks board. Cannot debug!</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785875#M31592</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Brendon, thank you. In fact I'm now doing what you suggested. I typically use the baseboard's buttons to temporarily change the boot mood.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Nov 2018 18:10:08 GMT</pubDate>
    <dc:creator>stuartrubin</dc:creator>
    <dc:date>2018-11-15T18:10:08Z</dc:date>
    <item>
      <title>LPC54018 IoT with SPIFI code in XIP bricks board. Cannot debug!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785871#M31588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing code which uses the SPIFI drivers to send commands to a flash device. The code must also run XIP. (I understand that this is problematic as code is being fetched from flash while I am simultaneously talking to the flash. I'm trying to work around that.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have programmed some code into flash which changes the flash controller (SPIFI), which subsequently crashes the program and hangs things up completely. Because the code is XIP, whenever I power-up the board, this code runs immediately.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that the code is preventing the debugger from working. I have tried both the LPC-Link 2 and Segger J-Link and they both have the same problem; the debugger cannot halt, or reset, or otherwise attach to the target. (See the debugger output listed below.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, how can I force the device to NOT run XIP, or at least keep it in a state where the debugger can connect and reprogram the flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to explicitly erase the flash, but I get the same problem. The debuggers / programmer cannot halt the target and connect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the output from degugger:&lt;/P&gt;&lt;P&gt;Could not connect to target.&lt;BR /&gt; SEGGER J-Link GDB Server V6.32b Command Line Version&lt;BR /&gt; JLinkARM.dll V6.32b (DLL compiled May 8 2018 18:26:33)&lt;BR /&gt; Command line: -nosilent -swoport 2332 -select USB=50116274 -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device LPC54018 -if SWD -halt -reportuseraction&lt;BR /&gt; -----GDB Server start settings-----&lt;BR /&gt; GDBInit file: none&lt;BR /&gt; GDB Server Listening port: 2331&lt;BR /&gt; SWO raw output listening port: 2332&lt;BR /&gt; Terminal I/O port: 2333&lt;BR /&gt; Accept remote connection: localhost only&lt;BR /&gt; Generate logfile: off&lt;BR /&gt; Verify download: on&lt;BR /&gt; Init regs on start: off&lt;BR /&gt; Silent mode: off&lt;BR /&gt; Single run mode: on&lt;BR /&gt; Target connection timeout: 0 ms&lt;BR /&gt; ------J-Link related settings------&lt;BR /&gt; J-Link Host interface: USB&lt;BR /&gt; J-Link script: none&lt;BR /&gt; J-Link settings file: none&lt;BR /&gt; ------Target related settings------&lt;BR /&gt; Target device: LPC54018&lt;BR /&gt; Target interface: SWD&lt;BR /&gt; Target interface speed: auto&lt;BR /&gt; Target endian: little&lt;BR /&gt; Connecting to J-Link...&lt;BR /&gt; J-Link is connected.&lt;BR /&gt; Device "LPC54018" selected.&lt;BR /&gt; Firmware: J-Link V10 compiled Apr 20 2018 16:47:09&lt;BR /&gt; Hardware: V10.10&lt;BR /&gt; S/N: 50116274&lt;BR /&gt; Feature(s): GDB&lt;BR /&gt; Checking target voltage...&lt;BR /&gt; Target voltage: 3.36 V&lt;BR /&gt; Listening on TCP/IP port 2331&lt;BR /&gt; Connecting to target...Found SW-DP with ID 0x2BA01477&lt;BR /&gt; Scanning AP map to find all available APs&lt;BR /&gt; AP[1]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt; AP[0]: AHB-AP (IDR: 0x24770011)&lt;BR /&gt; Iterating through AP map to find AHB-AP to use&lt;BR /&gt; AP[0]: Core found&lt;BR /&gt; AP[0]: AHB-AP ROM base: 0xE00FF000&lt;BR /&gt; CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)&lt;BR /&gt; Found Cortex-M4 r0p1, Little endian.&lt;BR /&gt; FPUnit: 6 code (BP) slots and 2 literal slots&lt;BR /&gt; CoreSight components:&lt;BR /&gt; ROMTbl[0] @ E00FF000&lt;BR /&gt; ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;BR /&gt; ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT&lt;BR /&gt; ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB&lt;BR /&gt; ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM&lt;BR /&gt; ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU&lt;BR /&gt; ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETM&lt;BR /&gt; Found SW-DP with ID 0x2BA01477&lt;BR /&gt; AP map detection skipped. Manually configured AP map found.&lt;BR /&gt; AP[0]: AHB-AP (IDR: Not set)&lt;BR /&gt; AP[0]: Core found&lt;BR /&gt; AP[0]: AHB-AP ROM base: 0xE00FF000&lt;BR /&gt; CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)&lt;BR /&gt; Found Cortex-M4 r0p1, Little endian.&lt;BR /&gt; FPUnit: 6 code (BP) slots and 2 literal slots&lt;BR /&gt; CoreSight components:&lt;BR /&gt; ROMTbl[0] @ E00FF000&lt;BR /&gt; ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;BR /&gt; ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT&lt;BR /&gt; ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB&lt;BR /&gt; ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM&lt;BR /&gt; ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU&lt;BR /&gt; ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETM&lt;BR /&gt; WARNING: CPU could not be halted&lt;BR /&gt; Halting target device failed. Trying again with reset&lt;BR /&gt; Failed to halt core before reset&lt;BR /&gt; WARNING: CPU could not be halted&lt;BR /&gt; Failed to halt target device on connect&lt;BR /&gt; ERROR: Could not connect to target.&lt;BR /&gt; Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...&lt;BR /&gt; Shutting down...&lt;BR /&gt; Could not connect to target.&lt;BR /&gt; Please check power, connection and settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 14:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785871#M31588</guid>
      <dc:creator>stuartrubin</dc:creator>
      <dc:date>2018-10-12T14:09:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 IoT with SPIFI code in XIP bricks board. Cannot debug!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785872#M31589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="307635" data-username="stuartrubin" href="https://community.nxp.com/people/stuartrubin"&gt;Stuart Rubin&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1. how can I force the device to NOT run XIP, or at least keep it in a state where the debugger can connect and reprogram the flash?&lt;BR /&gt;-- You can program and debug the demo in the RAM, however, it's necessary to adapt the linker file to make it.&lt;BR /&gt;I'd highly recommend you to refer to demos in the SDK library which contains a variety kind of demos for debugging.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 02:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785872#M31589</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-10-16T02:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 IoT with SPIFI code in XIP bricks board. Cannot debug!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785873#M31590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jeremtzhou, thank you for your response.  Unfortunately, the debugger cannot reset and halt the processor at all, so I cannot put a program into RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the only practical solution is connecting the module to a “baseboard” OM4006, the starting the board in ISP mode (pressing SW4). This cannot be done with the module alone without modifying the hardware. I have ordered the baseboard which should arrive today to confirm.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 15:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785873#M31590</guid>
      <dc:creator>stuartrubin</dc:creator>
      <dc:date>2018-10-16T15:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 IoT with SPIFI code in XIP bricks board. Cannot debug!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785874#M31591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC540xx boot ROM will attempt to execute code from flash by default, and if the&amp;nbsp;image found in flash is not valid then the ROM will disable debug and hence you cannot connect.&amp;nbsp;However it can be forced into ISP (in-System Programming) mode by pulling the ISP pins high or low, using the buttons available on the OM40006 or (much cheaper) OM40008 baseboards. The boot ROM samples these pins shortly after reset to determine what to do. There are various ISP modes (including UART/SPI/I2c and USB modes) that are defined by combination of the 3 ISP pins, but basically these allow you to program the device using one of the serial interfaces - see the chip User Manual for full details about device booting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other thing you can try is to mass erase the flash. The debug system might be able to get enough access to do this, although, depending on the code/data that is in the flash, this might not be possible. In MCUXpresso IDE you can use the GUI flash tool (the icon that looks like a chip on the tool bar, right next to the restart button). With your module connected, click on this button; if the tool is able to connect to your board then click on the Erase tab under the Target Operation section then select Mass Erase and click Run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even if you cannot fix your debug connection problems using Mass Erase, it is a useful way to clean things up when the flash content is messed up after you've "recovered" using ISP mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Nov 2018 16:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785874#M31591</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2018-11-15T16:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 IoT with SPIFI code in XIP bricks board. Cannot debug!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785875#M31592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Brendon, thank you. In fact I'm now doing what you suggested. I typically use the baseboard's buttons to temporarily change the boot mood.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Nov 2018 18:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-IoT-with-SPIFI-code-in-XIP-bricks-board-Cannot-debug/m-p/785875#M31592</guid>
      <dc:creator>stuartrubin</dc:creator>
      <dc:date>2018-11-15T18:10:08Z</dc:date>
    </item>
  </channel>
</rss>