<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error: Flash Download failed  -  Target DLL has been cancelled in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-Flash-Download-failed-Target-DLL-has-been-cancelled/m-p/785560#M31561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Have you been able to connect with the target at least once? You should verify the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Target processor is properly powered.&lt;/LI&gt;&lt;LI&gt;Debug connector from J-Link to target processor is properly mapped, oriented and connected.&lt;/LI&gt;&lt;LI&gt;The PC have installed the drivers for J-Link debugger.&lt;/LI&gt;&lt;LI&gt;Keil project configuration is properly set for the desired memory, included the related Flash driver file.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2018 22:43:23 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-11-21T22:43:23Z</dc:date>
    <item>
      <title>Error: Flash Download failed  -  Target DLL has been cancelled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-Flash-Download-failed-Target-DLL-has-been-cancelled/m-p/785559#M31560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Jlik to program LPC2148 in keil software. I am getting this error please help to overcome with this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Thippeswamy H U&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77721i37461D6CFDB20875/image-size/large?v=v2&amp;amp;px=999" title="error_jlink.png" alt="error_jlink.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 10:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-Flash-Download-failed-Target-DLL-has-been-cancelled/m-p/785559#M31560</guid>
      <dc:creator>swamy1</dc:creator>
      <dc:date>2018-11-21T10:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: Error: Flash Download failed  -  Target DLL has been cancelled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-Flash-Download-failed-Target-DLL-has-been-cancelled/m-p/785560#M31561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Have you been able to connect with the target at least once? You should verify the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Target processor is properly powered.&lt;/LI&gt;&lt;LI&gt;Debug connector from J-Link to target processor is properly mapped, oriented and connected.&lt;/LI&gt;&lt;LI&gt;The PC have installed the drivers for J-Link debugger.&lt;/LI&gt;&lt;LI&gt;Keil project configuration is properly set for the desired memory, included the related Flash driver file.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 22:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-Flash-Download-failed-Target-DLL-has-been-cancelled/m-p/785560#M31561</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-11-21T22:43:23Z</dc:date>
    </item>
  </channel>
</rss>