<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 4-bit ECC on LPC3250 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784564#M31521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a 4-bit ECC implementation for LPC3250?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with a new NAND flash with the NXP LPC3250. Previously a 1-bit ECC NAND was used and we moved to a 4-bit ECC NAND. It does not look like my U-Boot source supports 4-bit ECC. Does NXP have an implementation or example of U-Boot with 4-bit ECC support?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Sep 2018 18:28:45 GMT</pubDate>
    <dc:creator>speterson</dc:creator>
    <dc:date>2018-09-20T18:28:45Z</dc:date>
    <item>
      <title>4-bit ECC on LPC3250</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784564#M31521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a 4-bit ECC implementation for LPC3250?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with a new NAND flash with the NXP LPC3250. Previously a 1-bit ECC NAND was used and we moved to a 4-bit ECC NAND. It does not look like my U-Boot source supports 4-bit ECC. Does NXP have an implementation or example of U-Boot with 4-bit ECC support?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 18:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784564#M31521</guid>
      <dc:creator>speterson</dc:creator>
      <dc:date>2018-09-20T18:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: 4-bit ECC on LPC3250</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784565#M31522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Serah,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately No,&amp;nbsp; we do not have such solution for the LPC3250 since the device it is Legacy so the implementation for NAND flash with 4 bit ECC it is not available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for this inconvenience.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2018 16:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784565#M31522</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2018-10-24T16:14:46Z</dc:date>
    </item>
    <item>
      <title>Re: 4-bit ECC on LPC3250</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784566#M31523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/speterson"&gt;speterson&lt;/A&gt;&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jorge_plascencia"&gt;jorge_plascencia&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jamesbone"&gt;jamesbone&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;I have the same question, and am wondering what alternate approach was taken in Serah's case.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a need to implement 4-bit hardware ECC on a large block SLC NAND Flash because we are having issue with our software ECC.&amp;nbsp;If 4-bit ECC is not available, why does the UM10326 LPC32x0 manual indicate that the MLC controller can support 4-bit ECC?&amp;nbsp; We are trying to switch from the SLC to MLC controller for normal operations for this 4-bit ECC feature.&amp;nbsp; Are there any resources/code examples you can point me towards?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 20:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4-bit-ECC-on-LPC3250/m-p/784566#M31523</guid>
      <dc:creator>juan_castellano</dc:creator>
      <dc:date>2019-05-10T20:08:12Z</dc:date>
    </item>
  </channel>
</rss>