<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DEVICEID wrong address in UM10732 (LPC11U6x) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DEVICEID-wrong-address-in-UM10732-LPC11U6x/m-p/783363#M31468</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC_SYSCON-&amp;gt;DEVICID register is specified to be at offset 0x3F4 in the manual (UM10732), but it is actually located at offset 0x3F8. Reading LPC_SYSCON-&amp;gt;DEVICID thus does not yield a valid part ID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Workaround: The IAP function to read the part ID reads from the correct location, so just use this function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Source Code change: Change line 111 in syscon_11u6x.h to read:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;__I&amp;nbsp; uint32_t&amp;nbsp; RESERVED16[111];&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This moves the following DEVICEID field up to the correct offset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please change the address in the manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jul 2018 10:21:54 GMT</pubDate>
    <dc:creator>turboj</dc:creator>
    <dc:date>2018-07-25T10:21:54Z</dc:date>
    <item>
      <title>DEVICEID wrong address in UM10732 (LPC11U6x)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DEVICEID-wrong-address-in-UM10732-LPC11U6x/m-p/783363#M31468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC_SYSCON-&amp;gt;DEVICID register is specified to be at offset 0x3F4 in the manual (UM10732), but it is actually located at offset 0x3F8. Reading LPC_SYSCON-&amp;gt;DEVICID thus does not yield a valid part ID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Workaround: The IAP function to read the part ID reads from the correct location, so just use this function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Source Code change: Change line 111 in syscon_11u6x.h to read:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;__I&amp;nbsp; uint32_t&amp;nbsp; RESERVED16[111];&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This moves the following DEVICEID field up to the correct offset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please change the address in the manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 10:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DEVICEID-wrong-address-in-UM10732-LPC11U6x/m-p/783363#M31468</guid>
      <dc:creator>turboj</dc:creator>
      <dc:date>2018-07-25T10:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: DEVICEID wrong address in UM10732 (LPC11U6x)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DEVICEID-wrong-address-in-UM10732-LPC11U6x/m-p/783364#M31469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right, thank you for your feedback, I will report this to our documentation team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 13:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DEVICEID-wrong-address-in-UM10732-LPC11U6x/m-p/783364#M31469</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-07-25T13:30:50Z</dc:date>
    </item>
  </channel>
</rss>