<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB0_ID pin connection for USB0 in LPC4367 for non OTG application in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-ID-pin-connection-for-USB0-in-LPC4367-for-non-OTG/m-p/779489#M31355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This pin should be connected for an A-device (USB0_ID LOW), B-device (USB0_ID HIGH) or OTG this pin has an internal pull-up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jan 2018 18:32:53 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2018-01-12T18:32:53Z</dc:date>
    <item>
      <title>USB0_ID pin connection for USB0 in LPC4367 for non OTG application</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-ID-pin-connection-for-USB0-in-LPC4367-for-non-OTG/m-p/779488#M31354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using&amp;nbsp;&lt;A href="https://encrypted-tbn0.gstatic.com/images?q=tbn:ANd9GcQ1bVE7cw8A_THb0EWPM2lMC621aaJ_fhxvQkpjgBxMlrzMcIjp"&gt;USB Type-B&lt;/A&gt;&amp;nbsp;connector in our design and this connector has four pins D+, D-, VBUS and Ground and doesn't support OTG mode. USB0 of LPC4367 provides USB0_ID pin for OTG mode. For non-OTG mode can this pin be left open and can the USB connector be connected directly to the four pins namely D+, D-,&amp;nbsp; VBUS and ground or should the interface be moved to USB1 port of LPC4367 which doesn't have an ID pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 09:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-ID-pin-connection-for-USB0-in-LPC4367-for-non-OTG/m-p/779488#M31354</guid>
      <dc:creator>akhilesh_sreedh</dc:creator>
      <dc:date>2018-01-11T09:07:24Z</dc:date>
    </item>
    <item>
      <title>Re: USB0_ID pin connection for USB0 in LPC4367 for non OTG application</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-ID-pin-connection-for-USB0-in-LPC4367-for-non-OTG/m-p/779489#M31355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This pin should be connected for an A-device (USB0_ID LOW), B-device (USB0_ID HIGH) or OTG this pin has an internal pull-up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 18:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-ID-pin-connection-for-USB0-in-LPC4367-for-non-OTG/m-p/779489#M31355</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-01-12T18:32:53Z</dc:date>
    </item>
  </channel>
</rss>