<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4300 Boot Image Header question?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-Boot-Image-Header-question/m-p/779216#M31333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a LPC4370FET (flash-less, non AES part) that will be booted from its internal 128kB SRAM after loading the program image via USART0.&amp;nbsp; The User Manual (5.3.3) tells me I need to send a 16 byte Boot Image Header in Table 24;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;HASH_SIZE&lt;/STRONG&gt; is 16 bits – but my program image is &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;67 kB&lt;/STRONG&gt;&lt;/SPAN&gt; – how do I send the image size?&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;HASH_ACTIVE&lt;/STRONG&gt; could be 00 (reserved for non secure parts) or 11 (no hash is used) – which is correct for my non-AES part?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Dec 2017 11:55:33 GMT</pubDate>
    <dc:creator>davidgeorge</dc:creator>
    <dc:date>2017-12-11T11:55:33Z</dc:date>
    <item>
      <title>LPC4300 Boot Image Header question?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-Boot-Image-Header-question/m-p/779216#M31333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a LPC4370FET (flash-less, non AES part) that will be booted from its internal 128kB SRAM after loading the program image via USART0.&amp;nbsp; The User Manual (5.3.3) tells me I need to send a 16 byte Boot Image Header in Table 24;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;HASH_SIZE&lt;/STRONG&gt; is 16 bits – but my program image is &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;67 kB&lt;/STRONG&gt;&lt;/SPAN&gt; – how do I send the image size?&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;HASH_ACTIVE&lt;/STRONG&gt; could be 00 (reserved for non secure parts) or 11 (no hash is used) – which is correct for my non-AES part?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 11:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-Boot-Image-Header-question/m-p/779216#M31333</guid>
      <dc:creator>davidgeorge</dc:creator>
      <dc:date>2017-12-11T11:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4300 Boot Image Header question?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-Boot-Image-Header-question/m-p/779217#M31334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The answer is in Table 73 in section 7. It gives full description of the table items;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HASH_SIZE Size of the part of the image over which the hash value is&lt;BR /&gt;calculated in number of 512 Byte frames. Also size of the image copied to internal SRAM.&lt;BR /&gt;&lt;STRONG&gt;Hash size = 16[2] + HASH_SIZE x 512 Byte.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 12:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-Boot-Image-Header-question/m-p/779217#M31334</guid>
      <dc:creator>davidgeorge</dc:creator>
      <dc:date>2017-12-11T12:30:36Z</dc:date>
    </item>
  </channel>
</rss>