<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 temperature sensor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/temperature-sensor/m-p/775563#M31185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A while ago&amp;nbsp;&lt;A href="https://community.nxp.com/message/969158"&gt;https://community.nxp.com/message/969158&lt;/A&gt;&amp;nbsp;you told me that the WRAPEN field doesn't exist.&lt;/P&gt;&lt;P&gt;So, on page 491 of the LPC15 manual, it says&amp;nbsp;&lt;/P&gt;&lt;P&gt;"If the WRAPEN field is 0x2 the temperature sensor voltage is also output on the ADCn_0 pin"&lt;/P&gt;&lt;P&gt;In the absence of the WRAPEN field, would I find the temperature sensor voltage on the ADC pin, or not?&lt;/P&gt;&lt;P&gt;And presumably, it would only be there if the relevant bit in PINENABLE was set?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jun 2018 12:40:58 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2018-06-13T12:40:58Z</dc:date>
    <item>
      <title>temperature sensor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/temperature-sensor/m-p/775563#M31185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A while ago&amp;nbsp;&lt;A href="https://community.nxp.com/message/969158"&gt;https://community.nxp.com/message/969158&lt;/A&gt;&amp;nbsp;you told me that the WRAPEN field doesn't exist.&lt;/P&gt;&lt;P&gt;So, on page 491 of the LPC15 manual, it says&amp;nbsp;&lt;/P&gt;&lt;P&gt;"If the WRAPEN field is 0x2 the temperature sensor voltage is also output on the ADCn_0 pin"&lt;/P&gt;&lt;P&gt;In the absence of the WRAPEN field, would I find the temperature sensor voltage on the ADC pin, or not?&lt;/P&gt;&lt;P&gt;And presumably, it would only be there if the relevant bit in PINENABLE was set?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 12:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/temperature-sensor/m-p/775563#M31185</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2018-06-13T12:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: temperature sensor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/temperature-sensor/m-p/775564#M31186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just as I have told you, WRAPEN is just for the internal usage, customer can't use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Temperature sensor is connect to the ADC from internal, so I don't think you can test the temperature sensor voltage on the ADC pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please also check this register:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19111i7C0F762F1C3453A2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When you select the temperature to channel0, it won't select the ADCn_0 pin, so actually, to customer, there has no output pin for internal temperature sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2018 08:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/temperature-sensor/m-p/775564#M31186</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-06-14T08:46:28Z</dc:date>
    </item>
  </channel>
</rss>