<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCould not stop execution from running. Redlink error 255.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775225#M31169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How does one regain debugging control when this error occurs, without having to start the program from the beginning?&lt;/P&gt;&lt;P&gt;This is a common occurrence, due to the LPC-Link probe's poor EMC immunity - it happens when a contactor changes state, or even when the soldering iron thermostat turns off (or when a fly sneezes in the next office) and I am trying to monitor my program for an entire run-cycle of a week.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jun 2018 08:25:51 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2018-06-12T08:25:51Z</dc:date>
    <item>
      <title>Could not stop execution from running. Redlink error 255.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775225#M31169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How does one regain debugging control when this error occurs, without having to start the program from the beginning?&lt;/P&gt;&lt;P&gt;This is a common occurrence, due to the LPC-Link probe's poor EMC immunity - it happens when a contactor changes state, or even when the soldering iron thermostat turns off (or when a fly sneezes in the next office) and I am trying to monitor my program for an entire run-cycle of a week.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2018 08:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775225#M31169</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2018-06-12T08:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: Could not stop execution from running. Redlink error 255.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775226#M31170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could try attaching to the target, you can find more information on the chapter &lt;STRONG&gt;11.3.2 Connecting to a running Target&lt;/STRONG&gt; in the MCUXpresso IDE user guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the EMC inmunnity, does the same problems happen on other places besides the office? there seem to be many noise in your voltage line to cause what you mention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 20:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775226#M31170</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-06-18T20:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: Could not stop execution from running. Redlink error 255.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775227#M31171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hurrah for "attach" - that is a very useful feature! I can also see it being handy when a project starts correctly when launched by "debug", but doesn't when switched on from cold and allowed to start by itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The EMC immunity problems all stem from large inductances being de-energised. If the transformer in a Weller soldering iron on the same bench causes problems, what chance do I stand with the coil in a 160 Amp three-phase contactor? (It's definitely the coil, not the current being switched that causes problems) Both the USB and the SWD connections to the LPC-LINK2 are wound common-mode around a 40mm ferrite toroid, which improves things a lot, but it still fails with "bad ACK" from time to time when the contactor switches off.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 10:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Could-not-stop-execution-from-running-Redlink-error-255/m-p/775227#M31171</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2018-08-17T10:20:35Z</dc:date>
    </item>
  </channel>
</rss>