<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: QEI Digital filter related</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/QEI-Digital-filter-related/m-p/774116#M31122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All three encoder inputs (PhA, PhB, and index) require digital filtering. &lt;BR /&gt;The number of sample clocks is user programmable from 1 to 4,294,967,295 (0xFFFF FFFF).&lt;BR /&gt;The QEI Digital filter on phase A input register [FILTA] bits using to set the filter delay for phA input signal.&lt;BR /&gt;From below picture, the digital filter clock source is system clock.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11959iB4A278DD0C759DEB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For example:&lt;BR /&gt;If customer set the [FILTA] bits value to 0x10000 with system clock 72MHz, the filter delay will be 910us.&lt;BR /&gt;If customer set the [FILTA] bits value to 0x10000 with system clock 12MHz, the filter delay will be 5.5ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If customer want to filter the input glitch (200ns width), customer can set the [FILTA] bits value to 0x10 with system clock 72MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jun 2018 06:08:58 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2018-06-13T06:08:58Z</dc:date>
    <item>
      <title>QEI Digital filter related</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/QEI-Digital-filter-related/m-p/774115#M31121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;QIZ 1&amp;nbsp;&amp;nbsp; :&amp;nbsp; FILTA : Digital filter sampling delay ，&amp;nbsp; what kind of unit for FILTA?&lt;/P&gt;&lt;P&gt;QIZ2&amp;nbsp;&amp;nbsp;&amp;nbsp; :&amp;nbsp;&amp;nbsp;how to set&amp;nbsp; FILTA?&amp;nbsp; I need&amp;nbsp;a example of&amp;nbsp;application. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2018 06:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/QEI-Digital-filter-related/m-p/774115#M31121</guid>
      <dc:creator>yansinli</dc:creator>
      <dc:date>2018-06-12T06:40:18Z</dc:date>
    </item>
    <item>
      <title>Re: QEI Digital filter related</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/QEI-Digital-filter-related/m-p/774116#M31122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All three encoder inputs (PhA, PhB, and index) require digital filtering. &lt;BR /&gt;The number of sample clocks is user programmable from 1 to 4,294,967,295 (0xFFFF FFFF).&lt;BR /&gt;The QEI Digital filter on phase A input register [FILTA] bits using to set the filter delay for phA input signal.&lt;BR /&gt;From below picture, the digital filter clock source is system clock.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11959iB4A278DD0C759DEB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For example:&lt;BR /&gt;If customer set the [FILTA] bits value to 0x10000 with system clock 72MHz, the filter delay will be 910us.&lt;BR /&gt;If customer set the [FILTA] bits value to 0x10000 with system clock 12MHz, the filter delay will be 5.5ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If customer want to filter the input glitch (200ns width), customer can set the [FILTA] bits value to 0x10 with system clock 72MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 06:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/QEI-Digital-filter-related/m-p/774116#M31122</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-06-13T06:08:58Z</dc:date>
    </item>
  </channel>
</rss>