<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 lpc824 with lpcopen using uart and dma receive variable length data</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc824-with-lpcopen-using-uart-and-dma-receive-variable-length/m-p/773610#M31106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can somebody help me to achieve receiving the data which length is variable via uart (perhaps with dma?),thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Apr 2018 11:28:26 GMT</pubDate>
    <dc:creator>chengguozhang</dc:creator>
    <dc:date>2018-04-26T11:28:26Z</dc:date>
    <item>
      <title>lpc824 with lpcopen using uart and dma receive variable length data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc824-with-lpcopen-using-uart-and-dma-receive-variable-length/m-p/773610#M31106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can somebody help me to achieve receiving the data which length is variable via uart (perhaps with dma?),thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 11:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc824-with-lpcopen-using-uart-and-dma-receive-variable-length/m-p/773610#M31106</guid>
      <dc:creator>chengguozhang</dc:creator>
      <dc:date>2018-04-26T11:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: lpc824 with lpcopen using uart and dma receive variable length data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc824-with-lpcopen-using-uart-and-dma-receive-variable-length/m-p/773611#M31107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chengguo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPC824 apart of the LPCOpen has a code bundle. The code bundle does have a example of UART with DMA, also another good point of the code bundle is that the examples doesn't add so much overhead as the ones of the LPCOpen.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are working with MCUXpresso IDE you will find the code bundle in the next path:&lt;/P&gt;&lt;P&gt;C:\nxp\MCUXpressoIDE_10.1.1_606\ide\Examples\CodeBundles&lt;/P&gt;&lt;P&gt;In LPCXpresso the path is the following:&lt;/P&gt;&lt;P&gt;C:\nxp\LPCXpresso_8.2.2_650\lpcxpresso\Examples\CodeBundles&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 16:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc824-with-lpcopen-using-uart-and-dma-receive-variable-length/m-p/773611#M31107</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-04-30T16:13:23Z</dc:date>
    </item>
  </channel>
</rss>