<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Using TCPnet with KS8721 + LPC1768 + Keil</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-TCPnet-with-KS8721-LPC1768-Keil/m-p/519326#M3107</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Curious on Tue Aug 05 10:54:35 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i need to set up a &lt;/SPAN&gt;&lt;STRONG&gt;TCP/IP&lt;/STRONG&gt;&lt;SPAN&gt; or &lt;/SPAN&gt;&lt;STRONG&gt;UDP &lt;/STRONG&gt;&lt;SPAN&gt;network and config my board (lpc1768) as a &lt;/SPAN&gt;&lt;I&gt;client &lt;/I&gt;&lt;SPAN&gt;with a &lt;/SPAN&gt;&lt;STRONG&gt;KS8721 PHY IC&lt;/STRONG&gt;&lt;SPAN&gt;!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i changed &lt;/SPAN&gt;&lt;I&gt;[u]"PHY Identifier"[/u]&lt;/I&gt;&lt;SPAN&gt; to a ks8721 id and set &lt;/SPAN&gt;&lt;I&gt;[u]"PHY device address"[/u]&lt;/I&gt;&lt;SPAN&gt; with my board parameters (PHY Add. pins), setting Full-Duplex and 100Mb/s speed manually:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;write_PHY(PHY_REG_BMCR,0x2100); // Full Duplex - 100Mb/s&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;SPAN&gt;and at last comment the &lt;/SPAN&gt;&lt;I&gt;[u]link status checking[/u]&lt;/I&gt;&lt;SPAN&gt; code because KS8721 doesn't have the &lt;/SPAN&gt;&lt;I&gt;[u]PHY Status Register[/u]&lt;/I&gt;&lt;SPAN&gt; like dp83848 has!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Finally i could test &lt;/SPAN&gt;&lt;STRONG&gt;LEDClient &lt;/STRONG&gt;&lt;SPAN&gt;file (Keil\MCB1700\RL\TCPnet\LEDClient), UDP network connected and data sent to PC (sniffer it with Hercules_3.2.8 sw) from micro. &lt;/SPAN&gt;&lt;STRONG&gt;BUT &lt;/STRONG&gt;&lt;SPAN&gt;[color=#600]when i send anything from pc to micro, &lt;/SPAN&gt;&lt;STRONG&gt;udp_callback&lt;/STRONG&gt;&lt;SPAN&gt; doesn't call!!![/color]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;is there anything i should do more? or anyone who used [u]TCPnet with KS8721[/u]?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;tnx all&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;p.s: Excuse me for my bad english. &lt;SPAN class="lia-unicode-emoji" title=":slightly_smiling_face:"&gt;&lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:36:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:36:54Z</dc:date>
    <item>
      <title>Using TCPnet with KS8721 + LPC1768 + Keil</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-TCPnet-with-KS8721-LPC1768-Keil/m-p/519326#M3107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Curious on Tue Aug 05 10:54:35 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i need to set up a &lt;/SPAN&gt;&lt;STRONG&gt;TCP/IP&lt;/STRONG&gt;&lt;SPAN&gt; or &lt;/SPAN&gt;&lt;STRONG&gt;UDP &lt;/STRONG&gt;&lt;SPAN&gt;network and config my board (lpc1768) as a &lt;/SPAN&gt;&lt;I&gt;client &lt;/I&gt;&lt;SPAN&gt;with a &lt;/SPAN&gt;&lt;STRONG&gt;KS8721 PHY IC&lt;/STRONG&gt;&lt;SPAN&gt;!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i changed &lt;/SPAN&gt;&lt;I&gt;[u]"PHY Identifier"[/u]&lt;/I&gt;&lt;SPAN&gt; to a ks8721 id and set &lt;/SPAN&gt;&lt;I&gt;[u]"PHY device address"[/u]&lt;/I&gt;&lt;SPAN&gt; with my board parameters (PHY Add. pins), setting Full-Duplex and 100Mb/s speed manually:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;write_PHY(PHY_REG_BMCR,0x2100); // Full Duplex - 100Mb/s&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;SPAN&gt;and at last comment the &lt;/SPAN&gt;&lt;I&gt;[u]link status checking[/u]&lt;/I&gt;&lt;SPAN&gt; code because KS8721 doesn't have the &lt;/SPAN&gt;&lt;I&gt;[u]PHY Status Register[/u]&lt;/I&gt;&lt;SPAN&gt; like dp83848 has!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Finally i could test &lt;/SPAN&gt;&lt;STRONG&gt;LEDClient &lt;/STRONG&gt;&lt;SPAN&gt;file (Keil\MCB1700\RL\TCPnet\LEDClient), UDP network connected and data sent to PC (sniffer it with Hercules_3.2.8 sw) from micro. &lt;/SPAN&gt;&lt;STRONG&gt;BUT &lt;/STRONG&gt;&lt;SPAN&gt;[color=#600]when i send anything from pc to micro, &lt;/SPAN&gt;&lt;STRONG&gt;udp_callback&lt;/STRONG&gt;&lt;SPAN&gt; doesn't call!!![/color]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;is there anything i should do more? or anyone who used [u]TCPnet with KS8721[/u]?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;tnx all&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;p.s: Excuse me for my bad english. &lt;SPAN class="lia-unicode-emoji" title=":slightly_smiling_face:"&gt;&lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-TCPnet-with-KS8721-LPC1768-Keil/m-p/519326#M3107</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:36:54Z</dc:date>
    </item>
  </channel>
</rss>