<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Analog On Digital Port</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758759#M30570</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Hi,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;You only need to be careful with voltage and current maximum values. Regarding the voltage, if you configure the pin as a digital input,&amp;nbsp; then this pin takes as logical “high” level a 0.7VDD voltage value and for “low” level 0.3VDD voltage value.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;For example if VDD=3.3v&amp;nbsp; the level high minimum is 2.31v, and the maximum “low” level is 0.99v, for 1.8v you are in the threshold voltage.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;The max. current supported for digital pins is 10nA.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;I hope this helps,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Have a great day,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Sol&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jan 2018 22:53:52 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2018-01-03T22:53:52Z</dc:date>
    <item>
      <title>Analog On Digital Port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758758#M30569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On LPC11E14 I use PIO0_12 and PIO0_14 as encoder inputs.&amp;nbsp; As such these are both configured as digital inputs.&amp;nbsp; I would like to add broken cable detection, which would involve placing an analog voltage (VCC/2) on PIO0_12 and PIO0_14.&amp;nbsp; Then these pins would also connect to an analog input simultaneously.&amp;nbsp; Are there any consequences to placing the VCC/2 level on the digitally configured inputs?&amp;nbsp; Higher current drain perhaps?&amp;nbsp; Latch up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 17:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758758#M30569</guid>
      <dc:creator>mikenn</dc:creator>
      <dc:date>2018-01-03T17:40:45Z</dc:date>
    </item>
    <item>
      <title>Re: Analog On Digital Port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758759#M30570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Hi,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;You only need to be careful with voltage and current maximum values. Regarding the voltage, if you configure the pin as a digital input,&amp;nbsp; then this pin takes as logical “high” level a 0.7VDD voltage value and for “low” level 0.3VDD voltage value.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;For example if VDD=3.3v&amp;nbsp; the level high minimum is 2.31v, and the maximum “low” level is 0.99v, for 1.8v you are in the threshold voltage.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;The max. current supported for digital pins is 10nA.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;I hope this helps,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Have a great day,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Sol&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 22:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758759#M30570</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-01-03T22:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: Analog On Digital Port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758760#M30571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Whats up Soledad.&lt;/P&gt;&lt;P&gt;Just so I am clear, 10nA is the maximum input current on a digital input with input voltages of VCC, 0V, &lt;STRONG&gt;or VCC/2&lt;/STRONG&gt; ?&lt;/P&gt;&lt;P&gt;MikeN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 23:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758760#M30571</guid>
      <dc:creator>mikenn</dc:creator>
      <dc:date>2018-01-03T23:06:06Z</dc:date>
    </item>
    <item>
      <title>Re: Analog On Digital Port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758761#M30572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following values from the datasheet.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36634iD551D589AE51B9BA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 15:58:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Analog-On-Digital-Port/m-p/758761#M30572</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-01-04T15:58:48Z</dc:date>
    </item>
  </channel>
</rss>