<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC11xx ISO7816 T=1 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ISO7816-T-1/m-p/757905#M30482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leonardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the following application note and sample code for more information, it describes a USB CCID class smart card reader using an LPCXpresso LPC11U14 board. The sample project implements a smart card reader that conforms to ISO/IEC 7816 protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11121.zip"&gt;https://www.nxp.com/docs/en/application-note/AN11121.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Dec 2017 23:59:00 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2017-12-11T23:59:00Z</dc:date>
    <item>
      <title>LPC11xx ISO7816 T=1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ISO7816-T-1/m-p/757904#M30481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I want to use lpc1168 MCU for read/writing to/from V&lt;STRONG&gt;2.2.2&lt;/STRONG&gt; standard javacard,&lt;/P&gt;&lt;P&gt;As you know required clock signal is not produced by ISO7816 peripheral and match timer needed for generating this signal,I have 3 question:&lt;/P&gt;&lt;P&gt;1- As I tested match timer is not able to produce 3.5 mhz clock signal required for initialization steps,1mhz is best result I can generate,is there any one could achieve higher frequency?&lt;/P&gt;&lt;P&gt;2- As I know clock signal is used only for synchronization data ,then data must be fully&amp;nbsp;synchronized with clock signal ,but how this is possible in lpc11XX?I mean match timer generate clock signal automatically,and I send data over IO pin,but how&amp;nbsp; could I synchronized transmitted IO data with generated clock pin ?&lt;/P&gt;&lt;P&gt;3- Is there any tested ISO7816 sample,there are a sample for lpc11u14 which does not work and does not generate valid data ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Dec 2017 19:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ISO7816-T-1/m-p/757904#M30481</guid>
      <dc:creator>leonardorafaeli</dc:creator>
      <dc:date>2017-12-04T19:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11xx ISO7816 T=1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ISO7816-T-1/m-p/757905#M30482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leonardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the following application note and sample code for more information, it describes a USB CCID class smart card reader using an LPCXpresso LPC11U14 board. The sample project implements a smart card reader that conforms to ISO/IEC 7816 protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11121.zip"&gt;https://www.nxp.com/docs/en/application-note/AN11121.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 23:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ISO7816-T-1/m-p/757905#M30482</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-12-11T23:59:00Z</dc:date>
    </item>
  </channel>
</rss>