<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Why USART Master mode max. baudrate is higher than slave mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-USART-Master-mode-max-baudrate-is-higher-than-slave-mode/m-p/757437#M30471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sathwik,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I beleive this is because as a slave you will need the double of clock cycles to shift-in the data and respond to the master.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Mar 2018 16:56:38 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2018-03-08T16:56:38Z</dc:date>
    <item>
      <title>Why USART Master mode max. baudrate is higher than slave mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-USART-Master-mode-max-baudrate-is-higher-than-slave-mode/m-p/757436#M30470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Why USART Master mode max. baudrate is higher than slave mode max. baud rate?? &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Elaborately, I saw in every datasheet of LPC cortex-M controllers that, max. baud rate for USART in Synchronous master mode is higher (almost double) than USART in slave mode? Why that happened? Why USART can't give same max. speed in both master and slave modes? Is there any particular constraint? I wanted to know the reason because if I want to use same controller as USART master and slave I can't use max. baudrate of USART master becuase USART slave speed is low. So please explain the reason if anyone knows. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Thanks in advance.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jan 2018 10:36:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Why-USART-Master-mode-max-baudrate-is-higher-than-slave-mode/m-p/757436#M30470</guid>
      <dc:creator>TEMCEFF</dc:creator>
      <dc:date>2018-01-02T10:36:55Z</dc:date>
    </item>
    <item>
      <title>Re: Why USART Master mode max. baudrate is higher than slave mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-USART-Master-mode-max-baudrate-is-higher-than-slave-mode/m-p/757437#M30471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sathwik,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I beleive this is because as a slave you will need the double of clock cycles to shift-in the data and respond to the master.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Mar 2018 16:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Why-USART-Master-mode-max-baudrate-is-higher-than-slave-mode/m-p/757437#M30471</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-03-08T16:56:38Z</dc:date>
    </item>
  </channel>
</rss>