<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: OLED controller?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755369#M30414</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The controller supports the following types of LCD panel:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Active matrix TFT panels with up to 24-bit bus interface.&lt;/LI&gt;&lt;LI&gt;Single-panel monochrome STN panels (4-bit and 8-bit bus interface).&lt;/LI&gt;&lt;LI&gt;Dual-panel monochrome STN panels (4-bit and 8-bit bus interface per panel).&lt;/LI&gt;&lt;LI&gt;Single-panel color STN panels, 8-bit bus interface.&lt;/LI&gt;&lt;LI&gt;Dual-panel color STN panels, 8-bit bus interface per panel.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, you can connect an oled only if the oled has de same type of pins: RGB + HSYNC + VSYNC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Nov 2017 23:07:42 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2017-11-09T23:07:42Z</dc:date>
    <item>
      <title>OLED controller?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755368#M30413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the LPC4088 microcontroller, can the LCD controller be used for an OLED?&amp;nbsp; I see only TFT/STN in the user manual...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 17:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755368#M30413</guid>
      <dc:creator>markcianchetti</dc:creator>
      <dc:date>2017-11-07T17:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: OLED controller?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755369#M30414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The controller supports the following types of LCD panel:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Active matrix TFT panels with up to 24-bit bus interface.&lt;/LI&gt;&lt;LI&gt;Single-panel monochrome STN panels (4-bit and 8-bit bus interface).&lt;/LI&gt;&lt;LI&gt;Dual-panel monochrome STN panels (4-bit and 8-bit bus interface per panel).&lt;/LI&gt;&lt;LI&gt;Single-panel color STN panels, 8-bit bus interface.&lt;/LI&gt;&lt;LI&gt;Dual-panel color STN panels, 8-bit bus interface per panel.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, you can connect an oled only if the oled has de same type of pins: RGB + HSYNC + VSYNC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 23:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755369#M30414</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-11-09T23:07:42Z</dc:date>
    </item>
    <item>
      <title>Re: OLED controller?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755370#M30415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes it can be, but first better to know exactly &lt;A href="https://911electronic.com/oled-definition-what-is-oled/"&gt;what is oled&lt;/A&gt; couse in this situation oled structure is not good for that solution&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2018 19:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OLED-controller/m-p/755370#M30415</guid>
      <dc:creator>lamose2</dc:creator>
      <dc:date>2018-07-16T19:25:07Z</dc:date>
    </item>
  </channel>
</rss>