<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックhow do i use usart2 on a lpcxpresso4337?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-do-i-use-usart2-on-a-lpcxpresso4337/m-p/752546#M30289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use both usart0 and usart 2 for two different freertos tasks, but only usart0 sends/receives any message!&lt;/P&gt;&lt;P&gt;uart_init is set with LPC_USART2, USART0_IRQN and USART2_IRQHandler. uart cable connected to J2 pin 14. Help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 May 2018 14:00:53 GMT</pubDate>
    <dc:creator>erlendgrande</dc:creator>
    <dc:date>2018-05-14T14:00:53Z</dc:date>
    <item>
      <title>how do i use usart2 on a lpcxpresso4337?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-do-i-use-usart2-on-a-lpcxpresso4337/m-p/752546#M30289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use both usart0 and usart 2 for two different freertos tasks, but only usart0 sends/receives any message!&lt;/P&gt;&lt;P&gt;uart_init is set with LPC_USART2, USART0_IRQN and USART2_IRQHandler. uart cable connected to J2 pin 14. Help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 May 2018 14:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-do-i-use-usart2-on-a-lpcxpresso4337/m-p/752546#M30289</guid>
      <dc:creator>erlendgrande</dc:creator>
      <dc:date>2018-05-14T14:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: how do i use usart2 on a lpcxpresso4337?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-do-i-use-usart2-on-a-lpcxpresso4337/m-p/752547#M30290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erlend,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please notice in the schematic of the board that J2 pin 14 is not connected to anything.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8276iF6ADBDB66DB9161D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The pins you need to use for the UART2 are J2 13 and 15, that correspond to P2_10 and P2_11 respectively. If you reference the user manual:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/UM10503.pdf" title="https://www.nxp.com/docs/en/user-guide/UM10503.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM10503.pdf&lt;/A&gt;&amp;nbsp; In the page 310 you will see that both pins need to be set in function 2 in order to work with the UART2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 May 2018 17:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-do-i-use-usart2-on-a-lpcxpresso4337/m-p/752547#M30290</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-05-15T17:49:14Z</dc:date>
    </item>
  </channel>
</rss>