<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1549 CAN error problem.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751216#M30239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the problem is when this error is generated the error interrupt callback function&lt;/P&gt;&lt;P&gt;is called. the error code is 0x22.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i send again the data nothing happens the STAT register stills the same and&lt;/P&gt;&lt;P&gt;i have to reset the board to clear this register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Dec 2017 06:12:28 GMT</pubDate>
    <dc:creator>zakariatalebben</dc:creator>
    <dc:date>2017-12-28T06:12:28Z</dc:date>
    <item>
      <title>LPC1549 CAN error problem.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751214#M30237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am working on an LPC1549 dev board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i an using the CAN peripheral. the problem is when there is no a device&lt;/P&gt;&lt;P&gt;connected to CAN port and i send some data over the CAN port it will generate an ACK error&lt;/P&gt;&lt;P&gt;in the STAT register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but i am unable to reset the STAT register, even loading it with value 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there any mean to clear this register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Dec 2017 16:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751214#M30237</guid>
      <dc:creator>zakariatalebben</dc:creator>
      <dc:date>2017-12-27T16:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549 CAN error problem.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751215#M30238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zakaria Taleb Bendiab,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually in the LPC1549&amp;nbsp; STAT register description already give you answer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/34006iB72A1338CE8AAACE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/34058iF42649529E6B38DA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, don't care about the STAT ACKerror, after you send the CAN data successfully, these errors will be cleared automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 06:04:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751215#M30238</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-12-28T06:04:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549 CAN error problem.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751216#M30239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the problem is when this error is generated the error interrupt callback function&lt;/P&gt;&lt;P&gt;is called. the error code is 0x22.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i send again the data nothing happens the STAT register stills the same and&lt;/P&gt;&lt;P&gt;i have to reset the board to clear this register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 06:12:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-CAN-error-problem/m-p/751216#M30239</guid>
      <dc:creator>zakariatalebben</dc:creator>
      <dc:date>2017-12-28T06:12:28Z</dc:date>
    </item>
  </channel>
</rss>