<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: 7&amp;quot; LCD Hardware Design for LPC54608</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/7-quot-LCD-Hardware-Design-for-LPC54608/m-p/750859#M30234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC546xx and LPC540xx boards use an LCD panel that has a built-in touch panel controller. These MCUs do not have touch panel control circuits - you would need to add one of those to your design.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2018 15:32:43 GMT</pubDate>
    <dc:creator>brendonslade</dc:creator>
    <dc:date>2018-03-29T15:32:43Z</dc:date>
    <item>
      <title>7" LCD Hardware Design for LPC54608</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/7-quot-LCD-Hardware-Design-for-LPC54608/m-p/750858#M30233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to design my custom board and I will do somethings with lcd. Btw I chose Lpc54608. It has lcd and rtc options. I have 7"&amp;nbsp;tft panel&amp;nbsp;&lt;SPAN style="color: #484848; background-color: #ffffff; font-weight: bold;"&gt;SAT070CP40D21Y0351071KTP.&lt;/SPAN&gt;&lt;BR /&gt;You can see information about it in attachment. It is lil bit different from on board LCD panel on OM13092 eval board.&lt;BR /&gt;It has 40 pins. 37-40 pins are for touchscreen I think but I don't know which pins on Lpc54608 are for these 37-40 pins.&lt;BR /&gt;Is there any example for lcd connection and application note for this issue ?&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28183i77F33748840A5D3F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 14:19:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/7-quot-LCD-Hardware-Design-for-LPC54608/m-p/750858#M30233</guid>
      <dc:creator>fatihozen</dc:creator>
      <dc:date>2018-03-29T14:19:49Z</dc:date>
    </item>
    <item>
      <title>Re: 7" LCD Hardware Design for LPC54608</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/7-quot-LCD-Hardware-Design-for-LPC54608/m-p/750859#M30234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC546xx and LPC540xx boards use an LCD panel that has a built-in touch panel controller. These MCUs do not have touch panel control circuits - you would need to add one of those to your design.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 15:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/7-quot-LCD-Hardware-Design-for-LPC54608/m-p/750859#M30234</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2018-03-29T15:32:43Z</dc:date>
    </item>
  </channel>
</rss>