<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IAP commands not working after PLL set in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-commands-not-working-after-PLL-set/m-p/749872#M30192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Im using a lpc1549 and trying to use the IAP commands (particularly the eeprom read/write). This seems to work at the base 12MHz frequency, until I set the PLL to be 72MHz and set the main system clock to be PLL. It doesn't matter if I use the IAP setPLL function of my own bit twidding function.&amp;nbsp; Then calling an IAP command results in a hardware error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this mean I can't use the commands if running at full speed? or is there something I need to do ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Mar 2018 15:35:44 GMT</pubDate>
    <dc:creator>richardrobson</dc:creator>
    <dc:date>2018-03-12T15:35:44Z</dc:date>
    <item>
      <title>IAP commands not working after PLL set</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-commands-not-working-after-PLL-set/m-p/749872#M30192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Im using a lpc1549 and trying to use the IAP commands (particularly the eeprom read/write). This seems to work at the base 12MHz frequency, until I set the PLL to be 72MHz and set the main system clock to be PLL. It doesn't matter if I use the IAP setPLL function of my own bit twidding function.&amp;nbsp; Then calling an IAP command results in a hardware error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this mean I can't use the commands if running at full speed? or is there something I need to do ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 15:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-commands-not-working-after-PLL-set/m-p/749872#M30192</guid>
      <dc:creator>richardrobson</dc:creator>
      <dc:date>2018-03-12T15:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: IAP commands not working after PLL set</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-commands-not-working-after-PLL-set/m-p/749873#M30193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Richard,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just review the example of periph_iap provided in the LPCOpen, and the main system clock is set to 72MHz since the beginning and the example works fine. I recommend you to use this as a guide for your project to see which configurations you are missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Mar 2018 20:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-commands-not-working-after-PLL-set/m-p/749873#M30193</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-03-13T20:24:03Z</dc:date>
    </item>
  </channel>
</rss>